Skip to main content
rajesh23
Associate III
July 25, 2016
Question

USB mass storage

  • July 25, 2016
  • 1 reply
  • 556 views
Posted on July 25, 2016 at 09:02

Hi

i have configured the mass storage using cubemx,

but my code is not working it shows ''format disk to use'' in my system.

 here i have attached the configuration file 

can you any help me please.

regards

Rajesh

#sd-as-usb-mass-storage
This topic has been closed for replies.

1 reply

Walid FTITI_O
Visitor II
July 26, 2016
Posted on July 26, 2016 at 19:25

Hi d.rajesh.001,

Try to create on only thread for the same subject. Check the following response that I gave in this [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/STM32F746G-%20usb%20device%20mass%20storage%20with%20RTOS&currentviews=62]thread:

''

I have est the .ioc file that you shared , compile and generate code and everything is ok (no message as you indicated.

Check if you are using CubeMx 4.16.0 and Firmware package STM32Cube FW_F7 V1.4.1 version.

''

-Hannibal-