Skip to main content
rishi
Associate II
July 12, 2012
Question

USB Hub with stm32f4 discovery

  • July 12, 2012
  • 1 reply
  • 641 views
Posted on July 12, 2012 at 12:53

i have connected the usb hub to the discovery board using micro usb port...now i connected a pen drive 1 to the one port on hub...i want to do is when i connect another pen drive to the 2nd port on hub...the ucontroller will detect it and copy all the data from pendrive 1 to pendrive 2...so is it possible to do on discovery board??? if yes how,,

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    July 12, 2012
    Posted on July 12, 2012 at 22:00

    You might want to investigate if the part can host it that fashion, my understanding is that it isn't a full host implementation, and if you need a commercial USB stack.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..