Skip to main content
Bharat Kumar Bacha
Visitor II
March 6, 2018
Question

USB HS Host BenchMarks

  • March 6, 2018
  • 0 replies
  • 468 views
Posted on March 06, 2018 at 23:40

Did any one test USB-HS Host throughput benchmarks for both Tx and Rx?

In device mode i am getting around 120 Mbps (both tx and rx). Even STM replied that they are seeing the same speeds. But the results don't make sense for a 480 Mbps Speed USB as it is achieving only 25 percent of bandwidth.

Platform: STM32H743xi Eval Board

Thanks.

    This topic has been closed for replies.