Skip to main content
ssena.1514
Associate III
June 11, 2024
Solved

USB_HOST_MSC

Dear Sir/Madam,

I have already implemented the usb host mass storage class project which mainly mounts the usb disk & writes some data to a given file. But this application is not working. Only usb  unmout case is executing even though I am inserting the usb disk.

I am attaching the project files ,please check & reply me as soon as possible.

 

Software development environment - STM32cubeide

evaluation kit - stm32f401vc discovery kit

 

 

 

This topic has been closed for replies.
ssena.1514
ssena.1514Best answer
Associate III
July 5, 2024

Yes it is currently working. The problem was in the vbus.I had forgotten to configure vbus.

 

 

 

Thanks & Regards 

Satyabrata Senapati 

2 replies

ST Technical Moderator
July 4, 2024

Hi @ssena.1514 

Did you check the provided examples for MSC and having issue while enumerating the flash disk?

STM32CubeF4/Projects/STM324xG_EVAL/Applications/USB_Host/MSC_Standalone at master · STMicroelectronics/STM32CubeF4 (github.com)

Did you should check the protocol level using for example Wireshark?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
ssena.1514
ssena.1514AuthorBest answer
Associate III
July 5, 2024

Yes it is currently working. The problem was in the vbus.I had forgotten to configure vbus.

 

 

 

Thanks & Regards 

Satyabrata Senapati