Skip to main content
jonas239955
Associate II
December 5, 2012
Question

USB HID Linux

  • December 5, 2012
  • 0 replies
  • 622 views
Posted on December 05, 2012 at 10:43

Hi,

I do use the ST Evalboard STM3220G-Eval and started with ST example project USB HID Device Mouse/Joystick. It does work on Windows and Linux - no problems. Now I started to modify the example because my device should not appear as a mouse. I want to send 4 bytes of data from the usb device (Evalboard) to the usb host (computer). In file usbd_hid_core.c I did two changes: InterfaceProtocal was 2 and is now 0

0x00, 
/*nInterfaceProtocol : 0=none, 1=keyboard, 2=mouse*/

And the report descriptor looks like this

// HID_MOUSE_REPORT_DESC_SIZE = 21
0x06, 0x00, 0xff, 
// USAGE_PAGE (Vendor Defined Page 1)
0x09, 0x01, 
// USAGE (Vendor Usage 1)
0xa1, 0x01, 
// COLLECTION (Application)
0x15, 0x00, 
// LOGICAL_MINIMUM (0)
0x26, 0xff, 0x00, 
// LOGICAL_MAXIMUM (255)
0x75, 0x08, 
// REPORT_SIZE (8)
0x95, 0x04, 
// REPORT_COUNT (4)
0x09, 0x01, 
// USAGE (Vendor Usage 1)
0x81, 0x02, 
// INPUT (Data,Var,Abs)
0xc0 
// END_COLLECTION

In windows it does work and send 4 bytes of data. But with Linux I get an error during initialization: URB status: Broken pipe (-EPIPE) (-32) Does anyone know that problem?
    This topic has been closed for replies.