Skip to main content
pohua
Associate II
December 6, 2016
Question

USB HID Device Library or Example code

Posted on December 06, 2016 at 04:13

I want to create the USB HID device function but I don't have any library or example code.

Where to download the relation data for me reference?

PS:I use a STM32F427 MCU.
    This topic has been closed for replies.

    3 replies

    ST Technical Moderator
    December 6, 2016
    Posted on December 06, 2016 at 09:14

    Dear

    Chen.Pohua

    ‌

    ,

    To have more insight into the USB HID using the STM32Cube library, you can review the USB libraries and start from USB HID examples within the

    http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-embedded-software/stm32cubef4.html

    :

    STM32Cube_FW_F4_V1.0\Projects\STM324xG_EVAL\Applications\USB_Device

    You can refer also to the following documents:

    http://www.st.com/content/ccc/resource/technical/document/user_manual/b8/5a/28/c2/cf/b6/47/d6/DM00105pdf/files/DM00105pdf/jcr:content/translations/en.DM00105pdf

    : STM32Cube™ USB host library

    http://www.st.com/content/ccc/resource/technical/document/user_manual/cf/38/e5/b5/dd/1d/4c/09/DM00108pdf/files/DM00108pdf/jcr:content/translations/en.DM00108pdf

    : STM32Cube™ USB device library

    Best Regards

    -Imen-

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Radek RIPA
    ST Employee
    December 6, 2016
    Posted on December 06, 2016 at 09:34

    Hello

    You can look on this presentation labs. They are little older but there is described how to create the HID device with CubeMX

    Best regards

    Radek

    pohua
    pohuaAuthor
    Associate II
    December 12, 2016
    Posted on December 12, 2016 at 05:00

    Dear Imen and Radek:

    Thank you for your reply but I don't have an idea to develop my USB HID device because I use a standalone method to create my FW.

    I have referenced the STM32_USB-Host-Device_Lib_V2.2.0\Project\USB_Device_Examples\HID\src\usbd_desc, but I confuse the the descriptor doesn't include the descriptor description as configuration_descriptor, interface_descriptor, class_descriptor, endpoint_descriptor and HID Report descriptor.

    So I don't know how to create my HID device and the host can emulate the F427 to standard USB HID device?

    Do you have some examples for my reference?

    Thanks!

    Best Regards

    Pohua