Skip to main content
jbaron
Visitor II
March 13, 2013
Question

USB dual profile

Posted on March 13, 2013 at 22:23

Hi,

I have a project with a STM32F205 and I was wondering if I can have two USB profile loaded. I want to have the ''mass storage'' profile as well as the ''HID''.

Is it possible?

My second question is regarding the ''mass storage'' profile. Can I use the external NOR peripheral to share a memory through this profile.

Best regards,

Jerome

#stm32f205-usb
This topic has been closed for replies.

1 reply

dthedens23
Associate
March 14, 2013
Posted on March 14, 2013 at 15:48

''profile'' is a recognized USB term?

Do you mean you want a composite USB device that exposes two interfaces?  HID and MSD?

which USB stack are you using?

Composite devices are possible with careful attention to the USB descriptors, if the stack supports this feature.

STSW-STM32046 has a composite device example.

the second questions is harder.  You need to place a FAT,FAT16,FAT32  file system on the NOR flash.

What do you mean ''share''?  F2 code and USB device both read write NOR flash?  if so, somewhat harder.  FAT library must support multiple concurrent users.

If I had these requirements, I would specify that the system must have an RTOS.