Skip to main content
Mike Hooper
Associate III
December 5, 2017
Question

USB Device won't enumerate on custom F7 board

  • December 5, 2017
  • 0 replies
  • 422 views
Posted on December 05, 2017 at 15:34

I have a custom F7 board configured as a USB HID device (using CubeMX generated code) that won't enumerate with my PC host. However, if I pull BOOT0 high, it will enumerate as a 'STM Device in DFU Mode'. So I assume my hardware is working properly.

I have stepped through the initialization code and everything seems to be getting properly initialized (all functions return USBD_OK). However, there is no activity on the D+/D- lines as if they are not getting powered up.

Can anyone give some guidance on this?

Thanks,

    This topic has been closed for replies.