Question
USB device disconnect and connect in STM32L0
Posted on December 29, 2014 at 17:02
Hi
I just begin in STM32L0. I using my board for dev an USB example base STM32L053R8. And I have a confused about USB connect and disconnect. I run a test case based on STM32L053R8_NUCLEO_USB for test. And I don't want USB host detect USB device till I call function USBD_Start at the code below. But the Host still detect my USB device. I have check the bit DPPU (BCDR register). It is still disable. I can not Image what is the reason /* Init Device Library */ USBD_Init(&USBD_Device, &HID_Desc, 0); /* Register the HID class */ USBD_RegisterClass(&USBD_Device, &USBD_HID); while (1); /* Start Device Process */ USBD_Start(&USBD_Device);Thank for help. Kevin #stm32l0-usb-disconnect-connect