Skip to main content
Junde
Senior III
August 15, 2024
Solved

USB_DEVICE code can't work!

Hi there,

I am using STM32F429BIT6 and want to show the SDcard(connect with MCU by SDIO) as a Udisk on PC.

I can normally read/write the SD card by MCU with FATFS.

But after I added the USB config in CubeMx, the code is something wrong.

My CubeMX config is as follows:

Junde_0-1723691539237.png

Junde_1-1723691568096.pngJunde_2-1723691618953.pngJunde_3-1723691695548.png

Junde_4-1723692170702.png

As we can see, I enabled the USB log, but nothing output.

After debugging, I found the MCU is blocked in the while loop in USBD_GetEpDesc().

I don't know what that means, please help me. Thank you!

This topic has been closed for replies.
Junde
JundeBest answer
Senior III
August 22, 2024

Hi @FBL 

Thanks for your reply.

Finally I know the reason of mine project.

I am compiler the project with MDK compiler V6, this is NOT work for USB_DEVICE source code,

after I change to MDK compiler V5, everything is work well.

 

2 replies

ST Technical Moderator
August 21, 2024

Hi @Junde 

The issue with USBD_GetEpDesc() might be due to incorrect endpoint configuration. Would you share your endpoint descriptor config? Could you share a minimum project to reproduce?  USBD_MAX_STR_DESC_SIZ should be adjusted to accommodate the longest string descriptor you plan to use. A typical value might be 256 bytes to ensure USB stack can handle the string descriptors without buffer overflows. Also, it seems FH_mount(&sDisk[0]) is your custom initialization. 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Junde
JundeAuthorBest answer
Senior III
August 22, 2024

Hi @FBL 

Thanks for your reply.

Finally I know the reason of mine project.

I am compiler the project with MDK compiler V6, this is NOT work for USB_DEVICE source code,

after I change to MDK compiler V5, everything is work well.