Question
USB Communication Error
Posted on April 11, 2018 at 09:42
Hi,
strange problem here.
With STM32 ST-LINK Utility V4.10 & V4.20 i got an USB communication error with ST-Link/V2 Firmware V2J28S7, V2J29S7 and V2J30S7. With Version V2J30S7 and STM32 ST-LINK Utility V4.20 i got
OLD ST-LINK firmware/ST-LINK already used
under Settings.
With Firmware Version V2J23S4 i had not this problems.
I found this in the Trace Log.
SB communication error (65657) after target cmd F1 80 00 00 00 00 00 00 00 00
ST-Link get version failureThe detected STM32 firmware version (V0.J0) does not support the DAP read command.USB communication error (65657) after target cmd F1 80 00 00 00 00 00 00 00 00ST-Link get version failureThe detected STM32 firmware version (V0.J0) does not support the DAP read command.USB communication error (65657) after target cmd F1 80 00 00 00 00 00 00 00 00ST-Link get version failureThe detected STM32 firmware version (V0.J0) does not support the DAP read command.USB communication error (65657) after target cmd F1 80 00 00 00 00 00 00 00 00ST-Link get version failureThe detected STM32 firmware version (V0.J0) does not support the DAP read command.USB communication error (65657) after target cmd F1 80 00 00 00 00 00 00 00 00ST-Link get version failureThe detected STM32 firmware version (V0.J0) does not support the DAP read command.USB communication error (65657) after target cmd F1 80 00 00 00 00 00 00 00 00ST-Link get version failureThe detected STM32 firmware version (V0.J0) does not support the DAP read command.Thanks in advanced.
Sebastian