Skip to main content
albert_hsu
Associate II
November 24, 2008
Question

USB audio driver For STM32F103XX

  • November 24, 2008
  • 2 replies
  • 761 views
Posted on November 24, 2008 at 11:20

USB audio driver For STM32F103XX

    This topic has been closed for replies.

    2 replies

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:53

    Dear Albert,

    you do not need proprietary drivers to run Audio with STM32, the Provided Free USB kit uses Native Microsoft Drivers. Cheers,

    STone-32.

    albert_hsu
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:53

    Hi,

    Does ST provide USB audio driver for Window XP/Vista or Does ST use the standard protocols and no proprietary drivers are required? From the demo code downloaded from the website, I can find the drivers of mass storage device and virtual com port. But the demo code for the audio speaker doesn't need audio driver in PC. If I want to output digital audio to PC via USB, do I need to implement the proprietary audio driver for it?

    Thanks.

    Best regards,

    Albert.. :)