Skip to main content
jrupprecht9
Associate
December 16, 2008
Question

USART2 (RTS-Pin)

  • December 16, 2008
  • 1 reply
  • 700 views
Posted on December 16, 2008 at 06:51

USART2 (RTS-Pin)

    This topic has been closed for replies.

    1 reply

    jrupprecht9
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:56

    Hello,

    in the first, sorry for my bad english.

    I have make a Board wit h the STM32F103R8 and will use the

    PA01 as a Input-Pin (Switch) and use the USART2 as 2-Wire about Handshake.

    We use the IAR EWARM 5.2 and hthe STM-Lib 2.0

    My SW-Application is running without the usart-function. When i include the usart-function is the PA01 fix on high.

    my start-function:

    Init the GPIOs with GPIO-Clock (PA01 as IN_FLOATING

    Init the USART2 with USART-Clock and the GPIO´s TxD und RxD

    void Misc_Config(void)

    {

    GPIO_InitTypeDef GPIO_InitStructure;

    // IO-Vorbereitung

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB |

    RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD, ENABLE);

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;

    GPIO_Init(GPIOA, &GPIO_InitStructure);

    GPIO_Init(GPIOB, &GPIO_InitStructure);

    GPIO_Init(GPIOC, &GPIO_InitStructure);

    GPIO_Init(GPIOD, &GPIO_InitStructure);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB |

    RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | RCC_APB2Periph_AFIO, DISABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB |

    RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOD | RCC_APB2Periph_AFIO, ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

    ...

    // DI_TAST1

    GPIO_InitStructure.GPIO_Pin = DI_TAST1;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

    GPIO_Init(DI_TAST1_PORT, &GPIO_InitStructure);

    // DI_TAST2

    GPIO_InitStructure.GPIO_Pin = DI_TAST2;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

    GPIO_Init(DI_TAST2_PORT, &GPIO_InitStructure);

    }

    void USART_Config(void)

    {

    GPIO_InitTypeDef GPIO_InitStructure;

    USART_InitTypeDef USART_InitStructure;

    // USART init

    // USART Deinit

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

    USART_DeInit(USART2);

    GPIO_PinRemapConfig(GPIO_Remap_USART2,DISABLE);

    // Initialisiere Portpins

    // DO_RS232_TXD

    #if DO_RS232_TXD_FUNC == ALTERNATE

    GPIO_InitStructure.GPIO_Pin = DO_RS232_TXD;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

    GPIO_Init (DO_RS232_TXD_PORT, &GPIO_InitStructure);

    #endif

    // DI_RS232_RXD

    #if DI_RS232_RXD_FUNC == ALTERNATE

    GPIO_InitStructure.GPIO_Pin = DI_RS232_RXD;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

    GPIO_Init (DI_RS232_RXD_PORT, &GPIO_InitStructure);

    #endif

    USART_InitStructure.USART_BaudRate = 115200;

    USART_InitStructure.USART_WordLength = USART_WordLength_8b;

    USART_InitStructure.USART_StopBits = USART_StopBits_1;

    USART_InitStructure.USART_Parity = USART_Parity_No ;

    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

    // Configure the USART2

    USART_Init(USART2, &USART_InitStructure);

    // Enable the USART2

    USART_Cmd(USART2, ENABLE);

    } /* USART_Config */

    in Main

    // Init clock system

    RCC_Configuration();

    // NVIC configuration

    NVIC_Configuration();

    // Config Miscellaneous

    Misc_Config();

    // Config I2C-Bus

    I2C_Config();

    // Config USART2

    USART_Config();

    // External Interrupt Lines

    EXTI_Configuration();

    // Config AD-Converter

    ADC_Config();

    When i run the USART-Config goes the PA01 fix to high.

    The transmit is ok.

    Thanks for the help

    best regards

    Jörg