USART2 does n't work on STM32F302
Hello Everyone,
I am trying to send string on USART2 of STM32F302 but I am not succeed , my Code worked on USART1 and USART3. Does any one help me ?
#ifdef __GNUC__
/* With GCC/RAISONANCE, small printf (option LD Linker->Libraries->Small printf set to 'Yes') calls __io_putchar() */ #define PUTCHAR_PROTOTYPE int __io_putchar(int ch)#else #define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)#endif /* __GNUC__ */PUTCHAR_PROTOTYPE{ //Place your implementation of fputc here //e.g. write a character to the USART USART_SendData(USART2, (uint8_t) ch);//Loop until the end of transmission
while (USART_GetFlagStatus(USART2, USART_FLAG_TC) == RESET) {}return ch;
}void usart1_init (void)
{
USART_InitTypeDef USART_InitStructure;NVIC_InitTypeDef NVIC_InitStructure;
/* Bit configuration structure for GPIOC PIN4 and PIN5 */
GPIO_InitTypeDef GPIO_InitStructure;RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_7);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_7);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; // GPIO_Mode_OUT GPIO_Mode_AF GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_3; // GPIO_Speed_Level_2 GPIO_Speed_50MHz GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; // GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure);// Configure USART2 setting:
USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2,ENABLE);USART_ITConfig(USART2, USART_IT_RXNE, ENABLE);
NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);}
int main(void)
{ SystemInit(); gpio_init(); usart1_init (); // printf('Hello\n\r'); while (1){
printf('BIGS\n\r');
delay_ms(200); }}