Skip to main content
tran
Associate III
January 15, 2009
Question

USART1 et DMA cmd

  • January 15, 2009
  • 3 replies
  • 734 views
Posted on January 15, 2009 at 10:54

USART1 et DMA cmd

    This topic has been closed for replies.

    3 replies

    tran
    tranAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    Hello all!

    My situation is :i have a buffer TxBuffer[size] that i want transfer in USART1_DR by using DMA and then transfer it into an external device.

    But i can only do the transfer when i active the DMA_Cmd in the first time ( DMA and USART do it automtically). What i have to do if i want transfer one more times my buffer?

    Thanks

    tran
    tranAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    ok, it worked

    thanks you very much

    christophe239955_st
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 12:59

    You may use the DMA in Circular Mode. When circular mode is activated, the number of data to be transferred is automatically

    reloaded with the initial value programmed during the channel configuration phase, and the DMA requests continue to be served.

    This feature can be enabled using the CIRC bit in the DMA_CCRx register.

    Chris