Skip to main content
niklascooke2
Associate
July 4, 2009
Question

USART1 = dead!

  • July 4, 2009
  • 3 replies
  • 837 views
Posted on July 04, 2009 at 11:21

USART1 = dead!

    This topic has been closed for replies.

    3 replies

    niklascooke2
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:16

    Hi swhite!

    thank you so much!

    This line made my day GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; !!

    Ive been trying for a week now.

    Thank you again!

    Regards

    niklascooke2
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:16

    Hi everybody!

    Im wondering if someone got a clue what the problem could be,

    the Usart1 doesnt work at all. Ive tried everything!

    Im using Crossworks 1.7 with STM32F103CBT6.

    I get no signal mesured with a oscillscope.

    Clock are set but nothing happens!

    //Code

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOC | RCC_APB2Periph_GPIOB | RCC_APB2Periph_USART1, ENABLE);

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_Init(GPIOA, &GPIO_InitStructure);

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 ;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

    GPIO_Init(GPIOA, &GPIO_InitStructure);

    USART_InitTypeDef USART_InitStructure;

    USART_InitStructure.USART_BaudRate = 57600;

    USART_InitStructure.USART_WordLength = USART_WordLength_8b;

    USART_InitStructure.USART_StopBits = USART_StopBits_1;

    USART_InitStructure.USART_Parity = USART_Parity_No;

    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

    USART_Init(USART1, &USART_InitStructure);

    /* Enable USART1 */

    USART_Cmd(USART1, ENABLE);

    While(1){

    void SerialPutChar('a')

    {

    USART_SendData(USART1, c);

    while (USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET);

    }

    }

    Regards Niklas :o

    swhite
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:16

    Quote:

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

    Try changing the above line to

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

    Remember that peripheral outputs only connect to port pins when they're configured as an ''alternate function'' ;) Peripheral inputs always connect.

    You'll also need to enable the alternate function clock.

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);