Skip to main content
Valkan Pavlov
Associate III
May 9, 2023
Solved

USART with Nucleo L4R5ZI - bare metal/registry programming

Hey folks, I did try the bare metal programming videos on Udemy, and got so facinated, that decided to try on other board. As expected the code from the tutorial is not working on the other board. However I have checked, and re cheked the registry values that I provide, with the documentation of the correct board, and all seems to be OK, In addition to that I added 120 MHz for APB1 bus frequency, but I am still not getting anything on RealTerm.

In Udemy they do not respond to my questions, regarding other boards, so I really hope to get some help here. Thank you!

The device is Nucleo L4R5ZI, here is the code:

#include <stdint.h>
#include <stdio.h>
#include "stm32l4xx.h"
 
#define GPIOAEN 		(1U<<0)
#define UART2EN			(1U<<17)
 
 
#define SYS_FREQ 		120000000
#define APB1_CLK 		SYS_FREQ
 
#define CR1_TE 			(1U<<3)
#define CR1_UE			(1U<<0)
 
#define ISR_TXE 		(1U<<7)
 
 
static uint16_t compute_uart_div(uint32_t PeriphClk, uint32_t Baudrate);
 
static void uart_set_baudrate (USART_TypeDef *USARTx, uint32_t PeriphClk, uint32_t Baudrate);
 
static void uart2_write(uint8_t ch);
 
void uart2_tx_init (USART_TypeDef *USARTx);
 
 
int __io_putchar (int ch)
{
	uart2_write(ch);
	return ch;
}
 
int main(){
 
	uart2_tx_init (USART2);
 
	while (1)
	{
		printf ("Hello from STM32L4....\n\r");
	}
 
}
 
 void uart2_tx_init (USART_TypeDef *USARTx)
{
	//*******************Configure the UART pin*******************
	//Enable clock access to GPIOA for PA2 as TX line
	RCC->AHB2ENR |= GPIOAEN;
 
	//Set PA2 mode as alternate function mode
	GPIOA->MODER &=~(1U<<4);
	GPIOA->MODER |=(1U<<5);
 
	//Set the alternate function type to UART
	GPIOA->AFR[0] |=(1U<<8);
	GPIOA->AFR[0] |=(1U<<9);
	GPIOA->AFR[0] |=(1U<<10);
	GPIOA->AFR[0] &=~(1U<<11);
 
	//*******************Configure the UART module*******************
	//Enable clock access to UART2
	RCC->APB1ENR1 |=UART2EN;
 
	//Configure baudrate
	uart_set_baudrate (USARTx, APB1_CLK, 115200);
 
	//Configure transfer direction
	USARTx->CR1 = CR1_TE;
 
	// Enable UART module
	USARTx->CR1 |= CR1_UE;
}
 
static void uart2_write(uint8_t ch)
{
	//Wait for transmit data register to be empty
	while (!(USART2->ISR & ISR_TXE)) {}
 
	//Transmit value
	USART2->TDR = (ch & 0xFF);
 
}
 
 
static void uart_set_baudrate (USART_TypeDef *USARTx, uint32_t PeriphClk, uint32_t Baudrate)
{
	USARTx->BRR = compute_uart_div( PeriphClk, Baudrate);
}
 
static uint16_t compute_uart_div(uint32_t PeriphClk, uint32_t Baudrate)
{
	return ((PeriphClk + (Baudrate/2))/Baudrate);
}

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 9, 2023

Welcome, @Valkan Pavlov​, to the community!

The reason is probably that you have not adjusted the UART used for printf over the virtual COM port. The NUCLEO-L4R5ZI does not use UART2, but LPUART1.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

18 replies

Senior III
May 9, 2023

Do you compile it as C or C++?

Dudo
Valkan Pavlov
Associate III
May 9, 2023

C

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 9, 2023

Welcome, @Valkan Pavlov​, to the community!

The reason is probably that you have not adjusted the UART used for printf over the virtual COM port. The NUCLEO-L4R5ZI does not use UART2, but LPUART1.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Valkan Pavlov
Associate III
May 9, 2023

Hi Peter,

Thanks for the welcome, and the answer!

It was really the case, that LPUART1 is connected to the virtual COM port. I did try to set it up, and ended up with this:

#include <stdint.h>
#include <stdio.h>
#include "stm32l4xx.h"
 
 
 
#define GPIOGEN 		(1U<<6)
#define LPUART1EN		(1U<<0)
 
#define SYS_FREQ 		4000000 //It is 4MHz!
#define APB1_CLK 		SYS_FREQ
 
#define CR1_TE 			(1U<<3)
#define CR1_UE			(1U<<0)
 
#define ISR_TXE 		(1U<<7)
 
 
 
static uint16_t compute_LPUART_div(uint32_t PeriphClk, uint32_t Baudrate);
 
static void LPUART_set_baudrate (USART_TypeDef *LPUARTx, uint32_t PeriphClk, uint32_t Baudrate);
 
static void LPUART1_write(USART_TypeDef *LPUARTx, uint8_t ch);
 
void uart2_tx_init (USART_TypeDef *LPUARTx);
 
int __io_putchar (int ch)
{
	LPUART1_write(LPUART1, ch);
	return ch;
}
 
 
int main(){
 
	LPUART1_tx_init (LPUART1);
 
	while (1)
	{
		printf ("Hello from STM32L4....\n\r");
	}
 
}
 
 void LPUART1_tx_init (USART_TypeDef *LPUARTx)
{
	//*******************Configure the UART pin*******************
	//Enable clock access to GPIOG for PG7 as TX line
	RCC->AHB2ENR |= GPIOGEN;
 
	//Set PG7 mode as alternate function mode
	GPIOG->MODER &=~(1U<<14);
	GPIOG->MODER |=(1U<<15);
 
	//Set the alternate function type to TX - AF8
	GPIOG->AFR[0] &=~(1U<<28);
	GPIOG->AFR[0] &=~(1U<<29);
	GPIOG->AFR[0] &=~(1U<<30);
	GPIOG->AFR[0] |=(1U<<31);
 
	//*******************Configure the UART module*******************
 
	//Enable clock access to LPUART1
	RCC->APB1ENR2 |= LPUART1EN;
 
	//Configure baudrate ?????
	LPUART_set_baudrate (LPUART1, APB1_CLK, 115200); //?????
 
	//Configure transfer direction
	LPUART1->CR1 = CR1_TE;
 
	// Enable UART module
	LPUART1->CR1 |= CR1_UE;
 
 
}
 
static void LPUART1_write(USART_TypeDef *LPUARTx, uint8_t ch)
{
	//Wait for transmit data register to be empty
	while (!(LPUARTx->ISR & ISR_TXE)) {}
 
	//Transmit value
	LPUARTx->TDR = (ch & 0xFF);
}
 
 
static void LPUART_set_baudrate (USART_TypeDef *LPUARTx, uint32_t PeriphClk, uint32_t Baudrate)
{
	LPUARTx->BRR = compute_LPUART_div( PeriphClk, Baudrate);
}
 
static uint16_t compute_LPUART_div(uint32_t PeriphClk, uint32_t Baudrate)
{
	return ((PeriphClk + (Baudrate/2))/Baudrate);
}

It is not working, my baudrate formula is probably wrong, together with the SYS_FREQ that should be 32.768 MHz? If you have any more valuable advices, including learning resourses it will be greatly appreciated!

Thanks!

Senior III
May 11, 2023

You still init USART2, line 37

Dudo
Senior III
May 9, 2023

If the code that you paste is coplete, You use wrong sysclk value. After reset the board have used MSI oscilator and have set value around 4 MHz but you set 120 MHz without PLL configuration. Try set

#define SYS_FREQ 4000000

Your code works for me on this SYS_FREQ

Dudo
Valkan Pavlov
Associate III
May 9, 2023

Tx, yes it is complete. I did try with 120 MHz, 80MHz, 16MHz, and 4MHz. But I will try again with 4.

It id not work. Did you use it with the same board?

Senior III
May 9, 2023

I checked it on TeraTerm. Make sure for your COM settings, number of zeros in "clock define " etc :) Perhaps try reset board using button at the end

Dudo
Senior III
May 9, 2023

And look at @Peter BENSCH​ answer. You use UART through USB (ST-LINK) or from gold pins?

Dudo
Valkan Pavlov
Associate III
May 9, 2023

Yes, it requires some "dig" into documentation, so it was faster to check again with 4 I plan to do this now. I use the USB.

Senior III
May 9, 2023

LPUART1 is good choice :)

Dudo
Piranha
Principal III
May 13, 2023

> However I have checked, and re cheked the registry values that I provide

Again someone who defines their own register bit field definitions and uses magic numbers. Use the provided standard CMSIS definitions!