Skip to main content
rahul
Associate II
October 22, 2008
Question

usart usage

  • October 22, 2008
  • 4 replies
  • 832 views
Posted on October 22, 2008 at 09:08

usart usage

    This topic has been closed for replies.

    4 replies

    rahul
    rahulAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:48

    Hello freinds,

    I have been evaluating the STM32 controllers.

    So, I was trying out the driver for USART . All the configurations

    are shown correctly done in the keil software envoironment.

    But the communication doesn't take place.

    So, my first query would be that whether I need to enable UART interrupts essentially to make it work .

    Here I should mention that I was able to run the sample application code for Usart demonstration available on ST site which used interrupts .

    Any other recommendations are also welcome.

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:48

    Quote:

    I was trying out the driver for USART

    Which driver, exactly, were you trying?

    rahul
    rahulAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:48

    the library driver set provided on st site .

    It contains basic drivers for all the peripherals and description for the various functions is provided in the user manual for stm32f101xx family of controllers .

    [ This message was edited by: rahul.khurana on 20-10-2008 14:35 ]

    pt1
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:48

    Hi Rahul,

    I don't think that you need the USART interrupt enabled.

    Do you need an example? I've one with interrupt. It's a serial

    full-duplex communication.

    Best regards Edi