You are right. It's a bit different from the default idle line detection with its IDLE interrupt though, as it's a different feature with a separate interrupt (RTOF - Receiver Timeout). From the same RM0377:
Modbus/RTU [click "Show More"]
In this mode, the end of one block is recognized by a “silence�? (idle line) for more than 2 character times. This function is implemented through the programmable timeout function.The timeout function and interrupt must be activated, through the RTOEN bit in the USART_CR2 register and the RTOIE in the USART_CR1 register. The value corresponding to a timeout of 2 character times (for example 22 x bit duration) must be programmed in the RTO register. when the receive line is idle for this duration, after the last stop bit is received,an interrupt is generated, informing the software that the current block reception is completed.