Skip to main content
go_bare_foot
Associate
July 17, 2013
Question

USART_SendData adding bits

  • July 17, 2013
  • 2 replies
  • 681 views
Posted on July 17, 2013 at 11:42

Hey I'm running the STM32L1 chip with an XBEE unit and everything works perfectly except my Tx adds bits when there is an even number in the unsigned char (I typedef this as BYTE) being sent. Shows in Putty and X-CTU.

My code is:

void init_pkg( DWORD val, __IO BYTE* buff )

{

for ( int x = 0, len = TX_BUFF_SIZE - 1; x < len; x++ )

    {

        *buff++ = val + x;

    } 

    

    *buff++ = MSG_END_CHAR;

}

void xbee_IRQHandler( void )

{

// -- Send buffer EMPTY interrupt -- //    

    if ( (USART_GetITStatus( XBEE_USART, USART_IT_TXE )) != RESET )

    {

       delay( XBEE_SEND_TMOUT );  

        USART_SendData( XBEE_USART, (TxBuffer[ TxCounter ] & 0x7F) );

        

         if ( (++TxCounter) == TxBufferSize )                            

        {

            USART_ITConfig( XBEE_USART, USART_IT_TXE, DISABLE );        

        }

        

    }

}

Is there something i'm missing? I've checked the whole ASCII table and always adds a MSB when there's an even number of bits set.

Any help would be great as I'm lost.

Cheers

#discovery #stm32l #example-usart #xbee
This topic has been closed for replies.

2 replies

go_bare_foot
Associate
July 17, 2013
Posted on July 17, 2013 at 12:41

Sorry just found it, I'd got the parity bit setting wrong in the client side.

sanjib
Associate III
March 16, 2015
Posted on March 16, 2015 at 11:58

Hi

Can anybody say me how to configure for USARt half duplex in stm32l15cb  . I have configured as I configured for stm32f030(working USART half duplex) but it did not work what are the changes between stm32f030 and stm32l15cb