Skip to main content
arro239
Associate III
December 8, 2012
Question

USART: need CLOCK ticking all the time

  • December 8, 2012
  • 3 replies
  • 822 views
Posted on December 08, 2012 at 04:37

The device I am trying to connect to via serial interface requires constant clock ticking. I have enabled USART clock with

    USART_ClockInitTypeDef USART_ClockInitStructure;

    USART_ClockStructInit(&USART_ClockInitStructure);

    USART_ClockInitStructure.USART_Clock = USART_Clock_Enable;

    USART_ClockInit(USART2, &USART_ClockInitStructure);

but it seems to be ticking only while transmitting data. Is it possible to have this clock ticking constantly? I do not see any related fields in USART_ClockInitTypeDef

#usart
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
December 8, 2012
Posted on December 08, 2012 at 14:26

Not really.

Does this clock need to be synchronous to the serial signal? If not just use one of the timers to generate a continuous clock.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
arro239
arro239Author
Associate III
December 8, 2012
Posted on December 08, 2012 at 18:00

Wow :(

I have already implemented this via a timer but I was hoping this would only be an intermediate solution :( And the timer is obviously not in sync with the usart. While the chip does respond even like this is not cool, who knows if the chip will read control messages correctly all the time :( I guess I will implement TX via another timer channel to have them synched.

Different question while we are on the subject of times - is it possible to have an output channel and an input/capture channel configured on the same timer? I have spend some time trying to merge PWM_Input and PWM_Outout std examples to no avail.

Tesla DeLorean
Guru
December 8, 2012
Posted on December 09, 2012 at 00:22

Would SPI or I2S be a more suitable peripheral choice?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..