Skip to main content
hans5
Associate II
November 26, 2007
Question

USART in 9 bit mode with 2 stopbits?

  • November 26, 2007
  • 2 replies
  • 701 views
Posted on November 26, 2007 at 09:27

USART in 9 bit mode with 2 stopbits?

    This topic has been closed for replies.

    2 replies

    hans5
    hans5Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:18

    Hi,

    Tried it on an evaluation board and 9 databits in combination with 2 stopbits seems to work fine.

    So I assume it's a typo in the reference manual?

    regards, Hans

    hans5
    hans5Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:18

    Hi,

    For a specific application I want to use the USART in 9 databits mode in combination with 2 stopbits.

    The reference manual description of Control register 1 (USART_CR1) states that this combination is not possible:

    ''Bit 12 M: word length.

     

    This bit determines the word length. It is set or cleared by software.

     

    0: 1 Start bit, 8 Data bits, n Stop bit

     

    1: 1 Start bit, 9 Data bits, 1 Stop bit''

    In smartcard mode however, a setting is described with M=1 in combination with 1.5 stopbits:

    ''8 bits plus parity: where M=1 and PCE=1 in the USART_CR1 register and either:

     

    – 0.5 stop bits when receiving: where STOP=’01’ in the USART_CR2 register

     

    – 1.5 stop bits when transmitting: where STOP=’11’ in the USART_CR2 register.''

    Question:

    Is the number of stopbits in 9 bit datamode indeed limited to one?

    Thanks in advance for your answer!

    Hans Rosenbrand