USART HAL Tx Mirror on Rx
Hi!
I have a hardware setup with an RS485 in which all Tx Data is mirrored to Rx (no delay).
This simple example should echo all incoming chars coming from Rx back to Tx
If i do not use the delay in the callback before flushing DR the hardware mirrored Tx Data will not get flushed. - Sending one char to the Rx will end up in an endless loop of sending and receiving the same char.
So my question is:
Does HAL_UART_Transmit return before TC bit is set?
Any other explaination?
regards,
Walter
int main(void)
{
...
HAL_UART_Receive_IT(&huart1, &buffer, 1);
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
HAL_UART_Transmit(&huart1, &buffer, 1,0xff);
HAL_Delay(10);
/* If i do not use this delay there is a possibilty, that the UART data register will be filled up by
the mirrored Tx data after __HAL_UART_FLUSH_DRREGISTER
Open Questions regarding to this phenomenon:
Does HAL_UART_Transmit return before TC bit is set?
*/
__HAL_UART_FLUSH_DRREGISTER(&huart1);
HAL_UART_Receive_IT(&huart1, &buffer, 1);
}