Skip to main content
LMorr.3
Senior
June 10, 2023
Question

Upgrading CubeIDE1.9 to 1.12

I created many projects using CubeIDE1.9. I now installed CubeIDE1.12 and need to open my projects in the new version. I copied my old projects to a new workspace I created and then tried to import/open projects using CubeIDE1.12 but got a generic 'error' with no details when I try to open some of them.

How do I upgrade my projects from CubeIDE1.9 to CubeIDE1.12?

    This topic has been closed for replies.

    3 replies

    Pavel A.
    June 11, 2023

    More details please? Windows or Linux? Which STM32?

    Can you share an example project from CubeIDE 1.9?

    LMorr.3
    LMorr.3Author
    Senior
    June 12, 2023

    The issue was resolved. It was related to the .cproject file having been duplicated from another project without renaming the contents. CubeIDE1.12 would quit with an unknown error.

    I also had to use import 'Existing Projects into Workspace' instead of 'Projects from Folder or Archive'

    Pavel A.
    June 12, 2023

    Yes, this is not quite intuitive. When you want to import projects as is, without any conversion - use "Existing Projects into Workspace".

    But I rarely, if ever, had to edit .cproject files for renaming a project.

    Usually change of the name in .project file is enough.