Skip to main content
Visitor II
Apr 11, 2024 7:19 AM UTC
Question

Updating firmware via IO-Link

Hello,

I have a question regarding doing a firmware update via the USART-pins and IO-Link.

Would it be possible to use a IO-link master module to sent an update to the L6362A which translates it to 3.3V UART for the STM32G0B1KEU6 we are using in our current project.

I couldn't find anything about this. It seems possible but I would need some guidance.

We're using the UART1_pins. These allow for a firmware update on them. 

 

Thanks in advance!

 

This topic has been closed for replies.