Update from F4 to F7 -> Performance Problems
Hallo everybody,
i have a circuit board whitch is fitted with a STM32F429BIT.
The Software use STemWin and LWIP (without RTOS) and works good.
Now i has order the same circuit board with the pin compatible STM32F767BIT.
It is my first projekt with a F7.
Now i tested the LWIP with a terminal programm.
Then i tested STemWin. Also this worked perfectly.
But when I use both of them at the same time in the same code the LAN is very slow.
I have realised a tcp echo.
It sometimes takes up to 2 seconds until I get an answer.
I dont�t understand the Problem.
The AN4839 and AN4861 says that there is maybe a Problem with the DMA und the L1 Cache.
Maybe thats my problem. The solution is the use of the 'Managing memory protection unit (MPU)'.
I have init it as follows:
void MPU_Config(void)
{ MPU_Region_InitTypeDef MPU_InitStruct;/* Disables the MPU */
HAL_MPU_Disable(); /**Initializes and configures the Region and the memory to be protected */ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER0; MPU_InitStruct.BaseAddress = 0xC0000000; MPU_InitStruct.Size = MPU_REGION_SIZE_8MB; MPU_InitStruct.SubRegionDisable = 0x0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;HAL_MPU_ConfigRegion(&MPU_InitStruct);
/**Initializes and configures the Region and the memory to be protected
*/ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER1; MPU_InitStruct.BaseAddress = 0xC0000000; MPU_InitStruct.Size = MPU_REGION_SIZE_2MB; MPU_InitStruct.SubRegionDisable = 0x0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;HAL_MPU_ConfigRegion(&MPU_InitStruct);
/**Initializes and configures the Region and the memory to be protected
*/ MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER2; MPU_InitStruct.BaseAddress = 0x20020000; MPU_InitStruct.Size = MPU_REGION_SIZE_512KB; MPU_InitStruct.SubRegionDisable = 0x0; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);}
I have testet following possibilities:
I&DCache | MPU | Resultat ------------------------------------------------------------------- | | Lan very slow. -------------------------------------------------------------------- x | | lan not available . | | LTDC has sometimes flickering. --------------------------------------------------------------------- x | x | lan slightly faster | | LTDC has sometimes flickering. --------------------------------------------------------------------- | x | lan slightly faster ---------------------------------------------------------------------
Is the configuration of the MPU ok or is something entirely different to my problem?
#cache #f7 #mpu