Skip to main content
adaniel
Associate III
November 13, 2010
Question

Unique USB serial number for Stm32f103VB

  • November 13, 2010
  • 4 replies
  • 1234 views
Posted on November 13, 2010 at 09:38

Unique USB serial number for Stm32f103VB

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:14

    In the USB demo firmware from Stmicro, I can see that the USB serial number is built from the content of the memory locations at 1FFFF7E8, 1FFFF7EC and 1FFFF7F0, at the end of the system memory. My guess is that these locations hold a serial number unique for each chip. Since this not documented, can somebody confirm it?

    Like in the TRM?

    29.2 Unique device ID register (96 bits)

    The unique device identifier is ideally suited:

    �? for use as serial numbers (for example USB string serial numbers or other end

    applications)

    �? for use as security keys in order to increase the security of code in Flash memory while

    using and combining this unique ID with software cryptographic primitives and

    protocols before programming the internal Flash memory

    �? to activate secure boot processes, etc.

    The 96-bit unique device identifier provides a reference number which is unique for any

    device and in any context. These bits can never be altered by the user.

    The 96-bit unique device identifier can also be read in single bytes/half-words/words in

    different ways and then be concatenated using a custom algorithm.

    Base address: 0x1FFF F7E8

    Address offset: 0x00

    Read only = 0xXXXX where X is factory-programmed

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    adaniel
    adanielAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:14

    Thanks again, it is indeed there

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:14

    STM32 Reference Manual

    RM0008

    http://www.st.com/stonline/products/literature/rm/13902.pdf

    I recall some other details of wafer lot and die position, perhaps in the flash programmer code, but I'm not sure if that is remotely useful in the general case. The 96-bit number is supposed to be ST unique, but is not really suitable for a faux MAC address.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    adaniel
    adanielAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:14

    Many thanks! That exactly answers my question and also solves my problem. I am not at all concerned about security, I only need different serial numbers for several devices attached to the same computer.

     By the way, where did you find this information?