Skip to main content
enrico239955_st
Associate III
Aug 18, 2014 11:01 PM UTC
Question

unexpected behavior? not able to clear TIM_IT_Update

Posted on August 19, 2014 at 01:01

Hi, I am not able to clear a timer update flag while the timer is enabled. I am initializing a timer and the behavior is the following:

    ....

    TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure);

    TIM4->SR = (uint16_t)~TIM_IT_Update; // clear update flag

the flag was cleared

   ...

    TIM_Cmd(TIM4, ENABLE);

this sets all IT flags (update, cc1, cc2, cc3, cc4), why? I initialized cc1 with a large number, so it cant be hit by the initial counter value

    TIM4->SR = (uint16_t)~TIM_IT_Update; // clear update flag

the flag was NOT deleted

    TIM_Cmd(TIM4, DISABLE);

    TIM4->SR = (uint16_t)~TIM_IT_Update; // clear update flag

now the flag was deleted

What could be the reason for this behavior?
    This topic has been closed for replies.

    3 replies

    enrico239955_st
    Associate III
    Aug 18, 2014 11:33 PM UTC
    Posted on August 19, 2014 at 01:33

    ps: I am stepping through the code and I am watching the status flags after executing each line.

    enrico239955_st
    Associate III
    Aug 18, 2014 11:44 PM UTC
    Posted on August 19, 2014 at 01:44

    Is it possible that immediatly after clearing the flag the controller is setting the flag again (while debugging the timer is still running) so that I can not see the cleared flag?

    enrico239955_st
    Associate III
    Aug 18, 2014 11:54 PM UTC
    Posted on August 19, 2014 at 01:54

    Yes, that was the problem :)

    btw, I know that one can stop the timer while debugging the controller, but I use that seldom and I always forget the running timers..