Skip to main content
janvi2
Associate II
September 12, 2010
Question

understanding the connectivity clock tree

  • September 12, 2010
  • 1 reply
  • 799 views
Posted on September 12, 2010 at 23:39

understanding the connectivity clock tree

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    May 17, 2011
    Posted on May 17, 2011 at 14:06

    What is the diffrence between the signal PLLCLK and PLLVCO ?

    One is DOUBLE the other.

    My copy of RM0008 (Rev 11) clearly indicates that PLLVCO = 2 X PLLCLK, and that PLL3VCO = 2 * PLL3CLK

    The VCO (Voltage Controlled Oscillator) which the PLL is pumping up/down in frequency to achieve the desired rate using the HSI/HSE as a baseline reference. The VCO works at twice the PLL output to ensure that the mark/space ratio of the output clock is 50:50

    The PLL design is almost certainly capable of frequencies significantly higher than the logic portion of the STM32. I have ten year old CMOS SoC designs with PLL's in the 300 MHz region.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..