Skip to main content
Associate II
August 22, 2024
Solved

Understanding on Flash Memory Endurance Cycles for STM32 Microcontrollers

I’m using an STM32 microcontroller and am trying to understand more about the flash memory endurance cycles. The datasheet mentions an endurance of 1 kcycle (1,000 program/erase cycles). I think possible Write and read  (1000 cycles ) or is there any limits about  program/erase cycles?

Could  explain what exactly this means in terms of practical use? How are these cycles characterized, and what factors might affect the actual endurance in a real-world application?

 

 

 

Thanks!"

This topic has been closed for replies.
TDK
TDKBest answer
August 22, 2024

1 cycle = 1 erase + 1 write.

That means the chip will work if you erase and program it 1000 times. After that, operation is not guaranteed (but it's likely to continue to work well after that point).

 

The STM32G0x0 is a budget line. Lots of other families have 10k endurance cycles. If you have an application with lots of writing, perhaps look for a chip with higher endurance, or use an external dedicated FLASH chip.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
August 22, 2024

1 cycle = 1 erase + 1 write.

That means the chip will work if you erase and program it 1000 times. After that, operation is not guaranteed (but it's likely to continue to work well after that point).

 

The STM32G0x0 is a budget line. Lots of other families have 10k endurance cycles. If you have an application with lots of writing, perhaps look for a chip with higher endurance, or use an external dedicated FLASH chip.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
August 22, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.