Skip to main content
lizerd
Associate III
June 23, 2010
Question

undefined reference to `RCC_APB2PeriphClockCmd' Problem

  • June 23, 2010
  • 5 replies
  • 1816 views
Posted on June 23, 2010 at 23:17

undefined reference to `RCC_APB2PeriphClockCmd' Problem

    This topic has been closed for replies.

    5 replies

    John F.
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:55

    You also need to - Project (right click) ''Add Existing File'' stm32f10x_rcc.c to your project. Similarly if you use GPIO, add stm32f10x_gpio.c etc.

     

    swhite2
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:55

    You need to edit the ''stm32f10x_conf.h'' file and uncomment the #include statements for the peripherals you intent to use.

    John F.
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:55

    You probably need to define,

    USE_STDPERIPH_DRIVER

    You can do that in CrossWorks in the Solution or Project Properties - Preprocessor Options / Preprocessor Definitions. Decide first if you're going to set properties in the Solution or the Project and stick to it. I find it very easy to get confused with properties. Also, make sure you set Private / Common properties - don't change the Public Configurations.

    You can also set the STM32 type here (low med high) and do things like initialise the stack (see below). When you do get things working, you'll probably eventually overflow the stack. You can use the Symbol Browser Tool to see the stack then ''Locate Memory''.

    USE_STDPERIPH_DRIVER

    STM32F10X_HD

    INITIALIZE_STACK

    Use ST's Library html help for more info. Main Page, scroll down and click on ''How to use the Library''.

    Hope this works for you.

    John F.

    lizerd
    lizerdAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:55

    Hi and thanks.

    i get another error so i´m moving in the right direction i think =)

    now a get

    THUMB Flash Debug/stm32f10x_gpio.o: In function `GPIO_DeInit':

    C:/Users/Lizerd/Documents/CrossWorks Projects/test66/stm32f10x_gpio.c:110: undefined reference to `assert_param'

    THUMB Flash Debug/stm32f10x_gpio.o: In function `GPIO_Init':

    C:/Users/Lizerd/Documents/CrossWorks Projects/test66/stm32f10x_gpio.c:177: undefined reference to `assert_param'

    i have moved this files to project folder

    stm32f10x_rcc h and c

    stm32f10x_gpio h and c

    stm32f10x_conf.h

    stm32f10x.h

    i have include/link to

    stm32f10x_conf.h

    stm32f10x_gpio.c

    stm32f10x_rcc.c

    stm32f10x.h

    i have change stm32f10x_conf.h to

    /* Includes ------------------------------------------------------------------*/

    /* Uncomment the line below to enable peripheral header file inclusion */

    /* #include ''stm32f10x_adc.h'' */

    /* #include ''stm32f10x_bkp.h'' */

    /* #include ''stm32f10x_can.h'' */

    /* #include ''stm32f10x_cec.h'' */

    /* #include ''stm32f10x_crc.h'' */

    /* #include ''stm32f10x_dac.h'' */

    /* #include ''stm32f10x_dbgmcu.h'' */

    //#include ''stm32f10x_dma.h''

    //#include ''stm32f10x_exti.h''

    //#include ''stm32f10x_flash.h''

    //#include ''stm32f10x_fsmc.h''

    #include ''stm32f10x_gpio.h''

    /*#include ''stm32f10x_i2c.h''*/

    /* #include ''stm32f10x_iwdg.h'' */

    //#include ''stm32f10x_pwr.h''

    #include ''stm32f10x_rcc.h''

    /* #include ''stm32f10x_rtc.h'' */

    /* #include ''stm32f10x_sdio.h'' */

    //#include ''stm32f10x_spi.h''

    /* #include ''stm32f10x_tim.h'' */

    //#include ''stm32f10x_usart.h''

    /* #include ''stm32f10x_wwdg.h'' */

    //#include ''misc.h'' /* High level functions for NVIC and SysTick (add-on to CMSIS functions) */

    very thankful for all the help a can get, would be very happy if a can get this to compile without any errors.

    Best regards // Micke

    lizerd
    lizerdAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:55

    Yees finaly it works to compile without errors.

    Many Thanks // Micke