Skip to main content
saochandan
Associate
July 21, 2024
Solved

Unavailability of Exposed pad for STM32L031x4/6 in UFQFPN28 package

There is a note for UFQFPN32 package, that says "There is an exposed die pad on the underside of the UFQFPN package.", But there is no similar statement for UFQFPN28 package for the same device. Is it intentional or missed or if there is any plan to add if it is intentional?

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
July 21, 2024

Hello @saochandan 

This note concern only the UFQFPN48 and the UFQFPN32. The UFQFPN28 package is not concerned by the exposed pad so this note is not applicable in this case.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
July 21, 2024

Hello @saochandan 

This note concern only the UFQFPN48 and the UFQFPN32. The UFQFPN28 package is not concerned by the exposed pad so this note is not applicable in this case.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.