Skip to main content
dave4
Associate II
January 27, 2009
Question

unable to set bit

  • January 27, 2009
  • 12 replies
  • 1730 views
Posted on January 27, 2009 at 06:22

unable to set bit

    This topic has been closed for replies.

    12 replies

    dave4
    dave4Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    Hi,

    I am currently unable to set a bit on GPIOB, but I can reset it - here is the line of code

    GPIO_SetBits(GPIOB, GPIO_Pin_3);

    and here are the error messages the Keil compiler gives me:

    src\switch_output_on.c(75): error: #79: expected a type specifier

    src\switch_output_on.c(75): error: #79: expected a type specifier

    src\switch_output_on.c(75): error: #159: declaration is incompatible with previous ''GPIO_SetBits'' (declared at line 225 of ''.\libs\inc\stm32f10x_gpio.h'')

    My line 225 it references is here:

    void GPIO_SetBits(GPIO_TypeDef* GPIOx, u16 GPIO_Pin);

    As far as I can see, this should work, so what am I doing wrong here?

    --dave

    jilisegiar
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    Did you include the ''stm32f10x_lib.h'' file?

    jilisegiar
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    can you share the main.c file?

    dave4
    dave4Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    indeed, that is included.

    jj_it
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    Suggestion: ''kiss'' - modify the much smaller/simpler ''blinky'' program to output to your specified pin. (or even better - several additional ''same port'' pins) This seems faster/easier method...

    dave4
    dave4Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    Hi

    I'd rather not if thats ok, but here is the called function

    /**** Include files ****/

    #include ''stm32f10x_lib.h''

    #include ''stm32f10x_conf.h''

    #include ''stm32f10x_it.h''

    #include ''globals.h''

    #include

    #include ''parity.h''

    void switch_output_on(void)

    {

    /**** Variable declaration ****/

    static u8 char_count = 0; // message char count

    static u8 busy_semaphore = 0; // semaphore lock for tx

    u8 array_count = 0; // Array element counter

    vu8 message_on_contents[14];

    /**** typedefs ****/

    typedef struct

    {

    vu8 control_dollar;

    vu8 descriptor_p;

    vu8 descriptor_s;

    vu8 descriptor_u;

    vu16 address;

    vu8 space;

    vu8 command_o;

    vu8 command_p;

    vu8 command_uscore;

    vu8 command_e;

    vu8 command_n;

    vu8 CR;

    vu8 LF;

    } Send_msg_on;

    Send_msg_on MsgSend_on;

    /*** struct declaration ***/

    MsgSend_on.control_dollar = '$';

    MsgSend_on.descriptor_p = 'p';

    MsgSend_on.descriptor_s = 's';

    MsgSend_on.descriptor_u = 'u';

    MsgSend_on.address = psu_addr;

    MsgSend_on.space = 0x20;

    MsgSend_on.command_o = 'o';

    MsgSend_on.command_p = 'p';

    MsgSend_on.command_uscore = 0x5F;

    MsgSend_on.command_e = 'e';

    MsgSend_on.command_n = 'n';

    MsgSend_on.CR = 0x0D;

    MsgSend_on.LF = 0x0A;

    union message_on_union

    {

    vu8 message_on_contents[14];

    Send_msg_on MsgSend_on;

    }

    /**** Switch on outputs ****/

    GPIO_SetBits(GPIOB, GPIO_Pin_3);

    /**** Send message ****/

    MsgSend_on.address = psu_addr;

    if(busy_semaphore == 0)

    {

    busy_semaphore = 1; // set semaphore

    for(array_count=0;array_count<=14;array_count++)

    {

    if(USART_GetFlagStatus(USART1, USART_FLAG_TC) != RESET); // check TC flag set

    {

    USART_SendData(USART1, message_on_contents[array_count]); // send the set message to the UART

    char_count++;

    } // increment char counter

    }

    }

    busy_semaphore = 0; // reset semaphore

    }

    sorry if the formatting is messed up, when I tried to used code tags, all I got was a blank message

    --dave

    [ This message was edited by: dave6 on 21-01-2009 10:29 ]

    dave4
    dave4Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    thanks for the links, one problem though, I got the following error while trying to compile the second example

    Blinky.c(34): error: #20: identifier ''DMA_Channel1'' is undefined

    This is line 34

    DMA_Channel1->CMAR = (u32)&ADC_ConvertedValue;

    --dave

    jilisegiar
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    See at following path:

    C:\Keil\ARM\Boards\ST\STM32F10X_EVAL\Blinky

    C:\Keil\ARM\Boards\Keil\MCBSTM32\Blinky

    dave4
    dave4Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    as a slightly different way of thinking of this, how would I implement this without utilising the ST libraries, I'm beginning to think that for a simple thing like switching an IO on or off it would be more optimal to just code it without the libs.

    > modify the much smaller/simpler ''blinky'' program to output to your >specified pin.

    I had a look at that, thanks - but the code seems to be for the LPC2100 processor, is it the same code for the STM32, or does it require modifications?

    --dave

    [ This message was edited by: dave6 on 22-01-2009 10:25 ]

    jilisegiar
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    It compiles fine for me!