Skip to main content
Sm.2
Associate III
July 21, 2022
Question

Unable to receive complete data into my SPI slave receive buffer?

  • July 21, 2022
  • 0 replies
  • 450 views

I am using stm32h745zi-q board and I am working on the full duplex SPI. Here I aa using spi1 and spi4 . I used interrupt based at the spi1 means master side and I used DMA for SPI4 means slave side .

Here I am able to get the complete data in the SPI1 rx buffer but I am missing first 8characters in the SPI4 rx buffer where I used DMA.

Is there anything need to add to get the complete data in the spi4 rx buffer?

Thanks & Regards

SM.

This topic has been closed for replies.