Skip to main content
Associate
October 22, 2024
Solved

Unable to read stepsize of DAC

  • October 22, 2024
  • 1 reply
  • 568 views

I have configured DAC in nucleol496zg board using an internal voltage reference of scale around 2.048V , it is 12 bit DAC so step size would be around 0.5mv but when i write

 HAL_DAC_Start(&hdac1,DAC_CHANNEL_1);
 HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1,DAC_ALIGN_12B_R,0);

In multimeter it shows around 24.7mv-25mv for all the count values up to 25mv instead of step size DAC. Only if I give greater DAC count value (which produce above 25mv) it gives the correct millivolts in multimeter.

This topic has been closed for replies.
Best answer by waclawek.jan

You probably have the buffer on, in which case the output is not rail-to-rail. See VDAC_OUT parameter in the DAC characteristics table in datasheet.

Also mind the rather limited output current capability of the DAC, especially when buffer is off.

JW

1 reply

waclawek.jan
waclawek.janBest answer
Super User
October 22, 2024

You probably have the buffer on, in which case the output is not rail-to-rail. See VDAC_OUT parameter in the DAC characteristics table in datasheet.

Also mind the rather limited output current capability of the DAC, especially when buffer is off.

JW