Skip to main content
Vishnudev K
Associate II
April 8, 2018
Question

Unable to perform read in AT24c256

  • April 8, 2018
  • 9 replies
  • 1645 views
Posted on April 08, 2018 at 12:36

Iam trying to write and read to eeprom . I think i have wrote , in the code i have commended out the write function.

Now am trying to read, but the rxne is alwys reset

Please tell the correct usage of the functions for read and write

/**********************************************

*/

/* Includes ------------------------------------------------------------------*/

#include 'main.h'

#include 'stm32f0xx_rcc.h'

#include 'stm32f0xx_gpio.h'

#include 'stm32f0xx_i2c.h'

/** @addtogroup STM32F0xx_StdPeriph_Templates

* @{

*/

/* Private typedef -----------------------------------------------------------*/

#define EEPROM_ADDRESS_R 0xA1

#define EEPROM_ADDRESS_W 0xA0

#define EE_WRITE_ADDRESS 0x52AB

/* Private define ------------------------------------------------------------*/

/* Private macro -------------------------------------------------------------*/

/* Private variables ---------------------------------------------------------*/

uint8_t databuffer=0xAA;

char dataread;

/* Private function prototypes -----------------------------------------------*/

/* Private functions ---------------------------------------------------------*/

/**

* @brief Main program.

* @param None

* @retval None

*/

int main(void)

{

/*!< At this stage the microcontroller clock setting is already configured,

this is done through SystemInit() function which is called from startup

file (startup_stm32f0xx.s) before to branch to application main.

To reconfigure the default setting of SystemInit() function, refer to

system_stm32f0xx.c file

*/

/* Add your application code here

*/

//clocks enable

RCC_I2CCLKConfig(RCC_I2C1CLK_HSI);

RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2,ENABLE);

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB,ENABLE);

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC,ENABLE);

GPIO_InitTypeDef GPIO_InitStructure;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_1;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;

GPIO_Init(GPIOC,&GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_1;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;

GPIO_Init(GPIOC,&GPIO_InitStructure);

I2C_DeInit(I2C2);

GPIO_InitTypeDef I2C_GPIO_CONGIG;

I2C_GPIO_CONGIG.GPIO_Pin=GPIO_Pin_10;

I2C_GPIO_CONGIG.GPIO_Mode=GPIO_Mode_AF;

I2C_GPIO_CONGIG.GPIO_OType=GPIO_OType_OD;

I2C_GPIO_CONGIG.GPIO_PuPd=GPIO_PuPd_NOPULL;

I2C_GPIO_CONGIG.GPIO_Speed=GPIO_Speed_2MHz;

GPIO_Init(GPIOB,&I2C_GPIO_CONGIG);

//SCL

I2C_GPIO_CONGIG.GPIO_Pin=GPIO_Pin_11;

GPIO_Init(GPIOB,&I2C_GPIO_CONGIG);

//SDA

GPIO_PinAFConfig(GPIOB,GPIO_PinSource10,GPIO_AF_1);

GPIO_PinAFConfig(GPIOB,GPIO_PinSource11,GPIO_AF_1);

//I2C config

I2C_InitTypeDef I2C_InitStructure;

I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;

I2C_InitStructure.I2C_AnalogFilter = I2C_AnalogFilter_Enable;

I2C_InitStructure.I2C_DigitalFilter = 0x00;

I2C_InitStructure.I2C_OwnAddress1 = 0x00;

I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;

I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

I2C_InitStructure.I2C_Timing = 0x00201D2B;

// I2C_InitStructure.I2C_Timing = 0x1042C3C7;

I2C_Init(I2C2,&I2C_InitStructure);

//I2c enable

I2C_Cmd(I2C2,ENABLE);

//I2C_GenerateSTART(I2C2,ENABLE);

while(I2C_GetFlagStatus(I2C2, I2C_FLAG_BUSY) == SET)

{}

/* Configure slave address, nbytes, reload and generate start */

I2C_TransferHandling(I2C2, EEPROM_ADDRESS_W, 2, I2C_Reload_Mode, I2C_No_StartStop);

I2C_GenerateSTART(I2C2,ENABLE);

/* Wait until TXIS flag is set */

while(I2C_GetFlagStatus(I2C2, I2C_ISR_TXIS) == RESET)

{

}

/* Send MSB of memory address */

I2C_SendData(I2C2, (uint8_t)((EE_WRITE_ADDRESS & 0xFF00) >> 8));

/* Wait until TXIS flag is set */

while(I2C_GetFlagStatus(I2C2, I2C_ISR_TXIS) == RESET)

{

}

/* Send LSB of memory address */

I2C_SendData(I2C2, (uint8_t)(EE_WRITE_ADDRESS & 0x00FF));

/* Wait until TCR flag is set */

while(I2C_GetFlagStatus(I2C2, I2C_ISR_TCR) == RESET)

{GPIO_WriteBit(GPIOC,GPIO_Pin_9,Bit_SET);

}GPIO_WriteBit(GPIOC,GPIO_Pin_9,Bit_RESET);

//WRITE

// I2C_TransferHandling(I2C2, EEPROM_ADDRESS_W, 1, I2C_SoftEnd_Mode, I2C_No_StartStop);

//

// while(I2C_GetFlagStatus(I2C2, I2C_ISR_TXIS) == RESET)

// {

//

// GPIO_WriteBit(GPIOC,GPIO_Pin_8,Bit_SET);

// }

// GPIO_WriteBit(GPIOC,GPIO_Pin_8,Bit_RESET);

//

// I2C_SendData(I2C2, databuffer);

//

//READ

I2C_SlaveAddressConfig(I2C2,EEPROM_ADDRESS_W);

I2C_ReloadCmd(I2C2,DISABLE);

I2C_AutoEndCmd(I2C2,ENABLE);

I2C_NumberOfBytesConfig(I2C2,1);

I2C_MasterRequestConfig(I2C2,I2C_Direction_Receiver);

//Here i tried below function..it also didnt work//PLEASE HELP HERE

//I2C_TransferHandling(I2C2, EEPROM_ADDRESS_R, 1, I2C_SoftEnd_Mode, I2C_No_StartStop);

I2C_GenerateSTART(I2C2,ENABLE);

while(I2C_GetFlagStatus(I2C2, I2C_ISR_RXNE) == RESET)

{GPIO_WriteBit(GPIOC,GPIO_Pin_8,Bit_SET);

}

GPIO_WriteBit(GPIOC,GPIO_Pin_8,Bit_RESET);

/* Read data from RXDR */

dataread= I2C_ReceiveData(I2C2);

I2C_GenerateSTOP(I2C2,ENABLE);

/* Wait until STOPF flag is set */

while(I2C_GetFlagStatus(I2C2, I2C_ISR_STOPF) == RESET)

{GPIO_WriteBit(GPIOC,GPIO_Pin_9,Bit_SET);

} GPIO_WriteBit(GPIOC,GPIO_Pin_9,Bit_RESET);

/* Clear STOPF flag */

I2C_ClearFlag(I2C2, I2C_ICR_STOPCF);

while (1)

{

}

}

#ifdef USE_FULL_ASSERT

/**

* @brief Reports the name of the source file and the source line number

* where the assert_param error has occurred.

* @param file: pointer to the source file name

* @param line: assert_param error line source number

* @retval None

*/

void assert_failed(uint8_t* file, uint32_t line)

{

/* User can add his own implementation to report the file name and line number,

ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */

/* Infinite loop */

while (1)

{

}

}

#endif

/**

* @}

*/

Note: this post was migrated and contained many threaded conversations, some content may be missing.
    This topic has been closed for replies.

    9 replies

    Tesla DeLorean
    Guru
    April 8, 2018
    Posted on April 08, 2018 at 16:26

    Can we please not open multiple threads on materially the same topic

    https://community.st.com/0D50X00009XkWTtSAN

    Pretty sure the F0 doesn't require the address shift. The 0x50 looks to be appropriate. Review the EEPROM I2C example code provided in the F0 SPL

    I would suggest using a scope or logic-analyzer and confirming the signalling of address on the bus, and if the device responds with an ACK.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Vishnudev K
    Associate II
    April 8, 2018
    Posted on April 08, 2018 at 16:31

    what do you mean by addres shifting?

    Tesla DeLorean
    Guru
    April 8, 2018
    Posted on April 08, 2018 at 16:44

    Where the 7-bit Address is situated. On the bus it is the high order bits, ie 0xA0 == 0x50 << 1

    The examples for the F0 use 0x50, other STM32 families require you shift this. If you don't see the ACK on the bus it indicates no device recognizes the address you are using.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..