Question
Unable to initialise interrupts || Nucleo - F746ZG
Hi everyone,
I am new to the world of STM32 MCU's so please bear with me.
I am following a tutorial on Udemy and trying to write a GPIO interrupt code from scratch. I have done all register configurations and config is working fine as seen through SFR view in debug mode but when I run the code it seems like the interrupt is not enabled. The code never comes in the handler function.
#include <string.h>
#include "stm32f746xx.h"
#include "stm32f746xx_gpio_driver.h"
void delay(void){
for(uint32_t i=0; i<100000; i++);
}
int main(){
GPIO_PeriClockControl(GPIOC,ENABLE);
GPIO_PeriClockControl(GPIOB,ENABLE);
GPIO_Handle_t LED, BTN;
memset(&LED, 0, sizeof(LED));
memset(&BTN, 0, sizeof(BTN));
LED.pGPIOx = GPIOB;
LED.GPIO_PinConfig.GPIO_PinNumber = GPIO_PIN_NO_14;
LED.GPIO_PinConfig.GPIO_PinMode = GPIO_MODE_OUT;
LED.GPIO_PinConfig.GPIO_PinOPType = GPIO_OP_TYPE_PP;
LED.GPIO_PinConfig.GPIO_PinSpeed = GPIO_SPEED_VERY_HIGH;
LED.GPIO_PinConfig.GPIO_PinPuPdControl = GPIO_NO_PUPD;
GPIO_Init(&LED);
LED.pGPIOx = GPIOB;
LED.GPIO_PinConfig.GPIO_PinNumber = GPIO_PIN_NO_7;
LED.GPIO_PinConfig.GPIO_PinMode = GPIO_MODE_OUT;
LED.GPIO_PinConfig.GPIO_PinOPType = GPIO_OP_TYPE_PP;
LED.GPIO_PinConfig.GPIO_PinSpeed = GPIO_SPEED_VERY_HIGH;
LED.GPIO_PinConfig.GPIO_PinPuPdControl = GPIO_NO_PUPD;
GPIO_Init(&LED);
BTN.pGPIOx = GPIOC;
BTN.GPIO_PinConfig.GPIO_PinNumber = GPIO_PIN_NO_13;
BTN.GPIO_PinConfig.GPIO_PinMode = GPIO_MODE_IT_FT;
BTN.GPIO_PinConfig.GPIO_PinSpeed = GPIO_SPEED_VERY_HIGH;
BTN.GPIO_PinConfig.GPIO_PinPuPdControl = GPIO_PIN_PU;
GPIO_Init(&BTN);
//IRQ interrupt and priority configuration
GPIO_IRQPriorityConfig(IRQ_NO_EXTI10_15,NVIC_IRQ_PRIO_15);
GPIO_IRQIntConfig(IRQ_NO_EXTI10_15,ENABLE);
while(1);
}
void EXTI15_10_IRQHandle(void){
delay();
GPIO_IRQHandling(GPIO_PIN_NO_13);
GPIO_ToggleOutputPin(GPIOB,GPIO_PIN_NO_14);
GPIO_ToggleOutputPin(GPIOB,GPIO_PIN_NO_7);
}/*
* stm32f746xx_gpio_driver.c
*/
#include "stm32f746xx_gpio_driver.h"
/*
* peripheral clock setup
*/
void GPIO_PeriClockControl(GPIO_RegDef_t *pGPIOx, uint8_t EnOrDis){
if(EnOrDis == ENABLE){
if(pGPIOx == GPIOA){
GPIOA_PCLK_EN();
}else if(pGPIOx == GPIOB){
GPIOB_PCLK_EN();
}else if(pGPIOx == GPIOC){
GPIOC_PCLK_EN();
}else if(pGPIOx == GPIOD){
GPIOD_PCLK_EN();
}else if(pGPIOx == GPIOE){
GPIOE_PCLK_EN();
}else if(pGPIOx == GPIOF){
GPIOF_PCLK_EN();
}else if(pGPIOx == GPIOG){
GPIOG_PCLK_EN();
}else if(pGPIOx == GPIOH){
GPIOH_PCLK_EN();
}else if(pGPIOx == GPIOI){
GPIOI_PCLK_EN();
}else if(pGPIOx == GPIOJ){
GPIOJ_PCLK_EN();
}else if(pGPIOx == GPIOK){
GPIOK_PCLK_EN();
}
} else {
if(pGPIOx == GPIOA){
GPIOA_PCLK_DIS();
}else if(pGPIOx == GPIOB){
GPIOB_PCLK_DIS();
}else if(pGPIOx == GPIOC){
GPIOC_PCLK_DIS();
}else if(pGPIOx == GPIOD){
GPIOD_PCLK_DIS();
}else if(pGPIOx == GPIOE){
GPIOE_PCLK_DIS();
}else if(pGPIOx == GPIOF){
GPIOF_PCLK_DIS();
}else if(pGPIOx == GPIOG){
GPIOG_PCLK_DIS();
}else if(pGPIOx == GPIOH){
GPIOH_PCLK_DIS();
}else if(pGPIOx == GPIOI){
GPIOI_PCLK_DIS();
}else if(pGPIOx == GPIOJ){
GPIOJ_PCLK_DIS();
}else if(pGPIOx == GPIOK){
GPIOK_PCLK_DIS();
}
}
}
/*
* init and deInit
*/
void GPIO_Init(GPIO_Handle_t *pGPIOHandle){
uint32_t temp = 0;
if(pGPIOHandle->GPIO_PinConfig.GPIO_PinMode <= GPIO_MODE_ANALOG){
temp = (pGPIOHandle->GPIO_PinConfig.GPIO_PinMode << (2* pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber));
pGPIOHandle->pGPIOx->MODER &= ~(0x03 << pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber); // clearing ; always clear before setting
pGPIOHandle->pGPIOx->MODER |= temp; // setting
} else {
// 1. configure RTSR / FTSR
if(pGPIOHandle->GPIO_PinConfig.GPIO_PinMode == GPIO_MODE_IT_FT){
(*EXTI).FTSR |= (1<<pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber);
(*EXTI).RTSR &= ~(1<<pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber); // coz we only want FT, clear the corresponding RTSR bit; just to be safe if it is not already cleared for some reason
} else if(pGPIOHandle->GPIO_PinConfig.GPIO_PinMode == GPIO_MODE_IT_RT){
(*EXTI).RTSR |= (1<<pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber);
(*EXTI).FTSR &= ~(1<<pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber);
} else if(pGPIOHandle->GPIO_PinConfig.GPIO_PinMode == GPIO_MODE_IT_RFT){
(*EXTI).RTSR |= (1<<pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber);
(*EXTI).FTSR |= (1<<pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber);
}
// 2. config the gpio port selection in SYSCFG_EXTICR
uint8_t temp1 = pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber / 4;
uint8_t temp2 = pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber % 4;
uint8_t portcode = GPIO_BASEADDR_TO_CODE(pGPIOHandle->pGPIOx);
SYSCFG_PCLK_EN();
(*SYSCFG).EXTICR[temp1] = portcode << (temp2 * 4);
// 3. enable the exti interrupt delivery using IMR
(*EXTI).IMR |= (1<<pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber);
}
temp = 0;
temp = (pGPIOHandle->GPIO_PinConfig.GPIO_PinSpeed << (2* pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber));
pGPIOHandle->pGPIOx->OSPEEDR &= ~(0x03 << pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber); // clearing
pGPIOHandle->pGPIOx->OSPEEDR |= temp; // setting
temp = 0;
temp = (pGPIOHandle->GPIO_PinConfig.GPIO_PinPuPdControl << (2* pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber));
pGPIOHandle->pGPIOx->PUPDR &= ~(0x03 << pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber); // clearing
pGPIOHandle->pGPIOx->PUPDR |= temp; // setting
temp = 0;
temp = (pGPIOHandle->GPIO_PinConfig.GPIO_PinOPType << (pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber));
pGPIOHandle->pGPIOx->OTYPER &= ~(0x01 << pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber); // clearing
pGPIOHandle->pGPIOx->OTYPER |= temp; // setting
temp = 0;
if(pGPIOHandle->GPIO_PinConfig.GPIO_PinMode == GPIO_MODE_ALTFN){
uint8_t temp1 = pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber / 8;
uint8_t temp2 = pGPIOHandle->GPIO_PinConfig.GPIO_PinNumber % 8;
pGPIOHandle->pGPIOx->AFR[temp1] &= ~(0x0f << (4* temp2)); // clearing
pGPIOHandle->pGPIOx->AFR[temp1] |= pGPIOHandle->GPIO_PinConfig.GPIO_PinAltFunMode << (4* temp2); // setting
}
}
void GPIO_DeInit (GPIO_RegDef_t *pGPIOx){
if(pGPIOx == GPIOA){
GPIOA_REG_RESET();
}else if(pGPIOx == GPIOB){
GPIOB_REG_RESET();
}else if(pGPIOx == GPIOC){
GPIOC_REG_RESET();
}else if(pGPIOx == GPIOD){
GPIOD_REG_RESET();
}else if(pGPIOx == GPIOE){
GPIOE_REG_RESET();
}else if(pGPIOx == GPIOF){
GPIOF_REG_RESET();
}else if(pGPIOx == GPIOG){
GPIOG_REG_RESET();
}else if(pGPIOx == GPIOH){
GPIOH_REG_RESET();
}else if(pGPIOx == GPIOI){
GPIOI_REG_RESET();
}else if(pGPIOx == GPIOJ){
GPIOJ_REG_RESET();
}else if(pGPIOx == GPIOK){
GPIOK_REG_RESET();
}
}
/*
* data read and write
*/
uint8_t GPIO_ReadFromInputPin(GPIO_RegDef_t *pGPIOx, uint8_t PinNumber){
uint8_t value;
value = (uint8_t)((pGPIOx->IDR >> PinNumber) & 0x00000001);
return value;
}
uint16_t GPIO_ReadFromInputPort(GPIO_RegDef_t *pGPIOx){
uint16_t value;
value = pGPIOx->IDR;
return value;
}
void GPIO_WriteToOutputPin(GPIO_RegDef_t *pGPIOx, uint8_t PinNumber, uint8_t value){
if(value == GPIO_PIN_SET){
pGPIOx->ODR |= (1 << PinNumber);
} else if(value == GPIO_PIN_CLEAR || value == GPIO_PIN_RESET){
pGPIOx->ODR &= ~(1 << PinNumber);
}
}
void GPIO_WriteToOutputPort(GPIO_RegDef_t *pGPIOx, uint16_t value){
pGPIOx->ODR = value;
}
void GPIO_ToggleOutputPin(GPIO_RegDef_t *pGPIOx, uint8_t PinNumber){
pGPIOx->ODR ^= (1 << PinNumber);
}
/*
* IRQ configuration and ISR handling
*/
// IRQConfig is for config in processor side
void GPIO_IRQIntConfig(uint16_t IRQNumber, uint8_t EnOrDis){
if(EnOrDis == ENABLE){
// *(NVIC_ISER0 + (((uint32_t)(int32_t)IRQNumber) >> 5UL)) = (uint32_t)(1UL << (((uint32_t)(int32_t)IRQNumber) & 0x1FUL));
if(IRQNumber <= 31){
(*NVIC_ISER0) |= (1<<IRQNumber);
} else if((IRQNumber > 31) && (IRQNumber <= 63)){
(*NVIC_ISER1) |= (1<<(IRQNumber%32));
} else if((IRQNumber > 63) && (IRQNumber <= 95)){
(*NVIC_ISER2) |= (1<<(IRQNumber%64));
} else if(IRQNumber > 95){
(*NVIC_ISER3) |= (1<<(IRQNumber%96));
}
} else if (EnOrDis == DISABLE){
if(IRQNumber <= 31){
(*NVIC_ICER0) |= (1<<IRQNumber);
} else if((IRQNumber > 31) && (IRQNumber <= 63)){
(*NVIC_ICER1) |= (1<<(IRQNumber%32));
} else if((IRQNumber > 63) && (IRQNumber <= 95)){
(*NVIC_ICER2) |= (1<<(IRQNumber%64));
} else if(IRQNumber > 95){
(*NVIC_ICER3) |= (1<<(IRQNumber%96));
}
}
}
void GPIO_IRQPriorityConfig(uint16_t IRQNumber, uint16_t IRQPriority){
// 1. find the ipr register and section
uint32_t iprx = IRQNumber / 4;
uint32_t iprx_section = IRQNumber % 4;
// 2. store the value
uint8_t shift_value = (8*iprx_section) + (8-NO_IPR_BITS_IMPLEMENTED); // need to move more by (8-NO_IPR_BITS_IMPLEMENTED) bits, since not all of 8 bits are used..
uint16_t temp = (IRQPriority << shift_value);
*(NVIC_IPR_BASEADDR + iprx) |= temp; // iprx is multiplied by 4 because each address jump is of 4 bytes..
}
void GPIO_IRQHandling(uint8_t PinNumber){
// clear the exti pr register bit corresponding to the pin number
if((*EXTI).PR & (1<<PinNumber)){
(*EXTI).PR |= ( 1 << PinNumber );
}
}Please help me find the issue.
Thanks!