Hello M3allem. Thanks once again. For me it was an important point of the ADC max speed, as I did not know it. However, interrupt still did not occur. I do not wish to take further your time. Please, as a last help can you check that I configured channel A correctly?. Many thanks Johann
The ADC clock has to not excced 14MHz, so in your code the ADC clock works at 18MHz: /* PCLK2 = HCLK */ //hspeed bus 36MHz RCC_PCLK2Config(RCC_HCLK_Div1); /*ADCCLK = PCLK2/6 = 36/2 = 18MHz*/ RCC_ADCCLKConfig(RCC_PCLK2_Div2); So I think you have to replace RCC_PCLK2_Div2 by RCC_PCLK2_Div4 -> ADC clock = 36/4 = 9Mhz M3allem
Hekllo M3allem, Thanks once again. Please, if you have time can you check that I declared the clock well, because Im thinking that I have a setting not right. This is my code if you have time. Thanks,
void InitClk (void) //pg 262 { RCC_DeInit(); //resets RCC clock configuration to reset state. /* Enable HSE */ //External High Speed oscillator RCC_HSEConfig(RCC_HSE_ON); /* Wait till HSE is ready */ HSEStartUpStatus = RCC_WaitForHSEStartUp(); if(HSEStartUpStatus == SUCCESS) { RCC_HCLKConfig(RCC_SYSCLK_Div1); //AHB clock = SYSCLK //AHB is Advanced High-performance Bus, bus protocol. /*Flash 2 wait state */ FLASH_SetLatency(FLASH_Latency_2); /* Enable Prefetch Buffer */ FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); //PLLCLK = 8MHz / 2 = 4MHz * 9 = 36 MHz RCC_PLLConfig(RCC_PLLSource_HSE_Div2, RCC_PLLMul_9); //sets buses depending on internal clock limit is 36MHz, RM0008 pg 34 /* PCLK2 = HCLK */ //hspeed bus 36MHz RCC_PCLK2Config(RCC_HCLK_Div1); /* PCLK1 = HCLK *///lspeed bus 36Mhz limit is 36MHz RCC_PCLK1Config(RCC_HCLK_Div1); /*ADCCLK = PCLK2/6 */ RCC_ADCCLKConfig(RCC_PCLK2_Div2); /* Enable PLL */ RCC_PLLCmd(ENABLE); /*Wait till PLL is ready */ while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) {}; /* Select PLL as system clock source */ RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); /* Wait till PLL is used as system clock source */ while(RCC_GetSYSCLKSource() != 0x08) {}; } /* Enable DMA clock */ //DMA2 available on high density devices only RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); //RCC_AHBPeriphClockCmd(RCC_AHBPeriph_SRAM, ENABLE); /* ADC1 & 2 Periph clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); /* TIM1 Periph clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE); /* Enable GPIOA, GPIOB, GPIOC, GPIOD, GPIOE and AFIO clocks */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB , ENABLE); /* Enable USART1 clocks */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); // Enable SPI1 RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1,ENABLE); /* TIM2 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); // Enable SPI2 RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2,ENABLE); /* ADC1 & 2 Periph clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); }
Hello M3allem, Thanks a lot for your interest and for sending me the code. I will downloaded and go through it. I will notify you about my progress. Many thanks and have a nice day. Thanks Johann
Good morning M3allem. My problem is about the base address DMA_PeripheralBaseAddr. With ((u32)0x40012444C), was entering DMA2 and not DMA1. Im using the STM32F101x4 processor. DMA1 was being addressed after using (u32)ADC1_BASE as address. I will investigate some more and I will place all my code on the forum once ready. My problem is that it is not pointing to the address of the ADC result. I will keep you updated. Thanks Johann.