Skip to main content
Associate
May 8, 2026 3:43 AM UTC
Question

Unable to enter system bootloader STM32C071FBP6N

Hi,

As per title I am unable to enter the System Memory bootloader when using the STM32C071FBP6N. Any assistance would be greatly appreciated.

Following the notes in AN2606, i have configured pattern 11 (line 2) using the CubeProgrammer but when completing the reset with the Boot0 pin high it does not enter the bootloader mode and can tell this because my user application runs immediately after the reset occurs.

I have been able to jump to the bootloader through my own firmware where I initialize the HAL and GPIOs and then check the status of the boot0 or other pins then manually change the PC and SP but wish to avoid this method as this should not be necessary.

-------

I have followed the steps below:

1. Using a ST-Link I have successfully changed the option bits nBOOT_SEL=0; nBOOT1=1; nBOOT1=1; BOOT_LOCK=0 using the CubeProgrammer and have also flashed a basic UART output program which outputs to USART2 the whether the PA14/BOOT0/PA15 is high or low.

2. disconnect the ST-Link (since it interferes with the BOOT0 pin of this chip)

3. Set the BOOT0 pin high and then set nRST low then high

At this point i still see my application code running and output to the UART saying the PA14/BOOT0/PA15 is high

note: I am using minicom to read the UART and I have 'read' the option bit configurations to ensure they are properly saved on the device; Hardware-wise I am using a 10k Ohm pulldown resistor for the BOOT0 pin

11 replies

Associate
May 8, 2026 4:12 AM UTC

Any additional debugging ideas would also be great

ST Technical Moderator
May 11, 2026 10:50 AM UTC

Hello @NotThomasEdison 

I attempted to boot the device into the system bootloader using a Nucleo board, and the boot sequence works as expected on my setup.

Please take a look to the schematic of NUCLEO-C071RB

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
EThom.3
Senior II
May 11, 2026 11:28 AM UTC

What do you use for setting BOOT0 high? A mechanical switch?

Do you see any difference whether you set nRST low and high, or if you power cycle the microcontroller?

ST Technical Moderator
May 11, 2026 1:09 PM UTC

@EThom.3 wrote:

What do you use for setting BOOT0 high? A mechanical switch?


I used the boot mode button which set the pin BOOT0 to high.

Saket_Om_0-1778504809934.png

I click on boot mode button to set BOOT0 pin high then click on reset button. 

Saket_Om_1-1778504953266.png

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
EThom.3
Senior II
May 11, 2026 1:16 PM UTC

> I click on boot mode button to set BOOT0 pin high then click on reset button.

Ah! I had missed that you were using a Nucleo board. Sorry.

Try holding the boot mode button pressed while you click the reset button. If you click and release the boot button before you press the reset button, the BOOT0 pin will no longer be high when you reset.