Question
UART4 DMA Rx Problem
Posted on April 04, 2014 at 13:21
I cannot get into DMA mode, the code I wrote did not get into DMA interrupt. The code I wrote is as follows. Any advice?( my processor is STM32F103ZG)
uint8_t RxBuffer1[100]; /*UART - Pin Config*/ GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; DMA_InitTypeDef DMA_InitStructure;; /* Clock configuration -------------------------------------------------------*/ RCC_APB2PeriphClockCmd( UART_GPIO_CLK_TX | UART_GPIO_CLK_RX | RCC_APB2Periph_AFIO, ENABLE); RCC_APB1PeriphClockCmd(UART_CLK , ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA2,ENABLE); /* Configure the GPIO ports( UART4 Transmit and Receive Lines) */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Pin = UART_TxPin; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(UART_GPIO_TX, &GPIO_InitStructure); /* Configure the UART4_Rx as input floating */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_InitStructure.GPIO_Pin = UART_RxPin ; GPIO_Init(UART_GPIO_RX, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 1200; USART_InitStructure.USART_WordLength = USART_WordLength_9b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_Even; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; /* UART Guard Time set to 16 Bit */ USART_SetGuardTime(UART4, 8); USART_Init(UART4, &USART_InitStructure); /* Enable the UART4 */ USART_Cmd(UART4, ENABLE); /************************* DMA *****************************/ DMA_DeInit(DMA2_Channel3); DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&UART4->DR; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)RxBuffer1; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; // Receive DMA_InitStructure.DMA_BufferSize = 1; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA2_Channel3, &DMA_InitStructure); /* Enable the USART Rx DMA request */ USART_DMACmd(UART4, USART_DMAReq_Rx, ENABLE); /* Enable DMA Transfer Complete interrupt */ DMA_ITConfig(DMA2_Channel3, DMA_IT_TC, ENABLE); /* Enable the DMA RX Stream */ DMA_Cmd(DMA2_Channel3, ENABLE); /* Enable the UART4 RX DMA Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = DMA2_Channel3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /*******************************************************************/ void DMA2_Channel3_IRQHandler(){ if(DMA_GetITStatus(DMA2_IT_TC3)){ Uart_Interrupt_Handler(); DMA_ClearITPendingBit(DMA2_IT_TC3); }