Skip to main content
semed abubakar
Associate II
March 28, 2018
Question

uart with interrupt stm32L4

  • March 28, 2018
  • 1 reply
  • 729 views
Posted on March 28, 2018 at 13:02

trying to set up a UART  receive with interrupt so far no success code is below im using stm32l4

any suggestions would be great thanks

#include 'stm32l4xx.h'

#include 'stm32l433xx.h'

char uart3_tx_data[]=' is here again';

void Init_USART3();

int indexx;

char usart3_rcv_buffer[20];

void USART3_IRQHandler()

{

Toogle_GPIOB_Pin(9);

if ((USART1->ISR & USART_ISR_RXNE) == USART_ISR_RXNE)

{

send_string(usart3_rcv_buffer);

usart3_rcv_buffer[indexx++] = (USART3->RDR); /* Receive data, clear flag */

}

}

int main (void)

{

RCC->APB1ENR1 |=(1<<4); //TIM6 clock enabled

TIM6->PSC = 0; // f timer = fclk / 24000 => 1kHz

TIM6->ARR = 0xFFf;

TIM6->CR1 = TIM_CR1_CEN;

RCC->AHB2ENR |= RCC_AHB2ENR_GPIOBEN;

RCC->AHB2ENR |= RCC_AHB2ENR_GPIOCEN;

RCC->AHB2ENR |= RCC_AHB2ENR_GPIOAEN;

GPIOC ->MODER &= ~ GPIO_MODER_MODE10_0;                        ///set GPIO2 as alternate functions

GPIOC ->MODER |= (GPIO_MODER_MODE10_1);

GPIOC ->OTYPER &= ~(GPIO_OTYPER_OT_10)                 ; ///push pull output type for GPIOA12

GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR10_0); // high speed for GPPIOC12

GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR10_1);

GPIOC ->PUPDR &= ~(GPIO_PUPDR_PUPDR10); //NO PULL UP*/

GPIOC ->MODER &= ~ GPIO_MODER_MODE11_0;                       ///set GPIO2 as alternate functions

GPIOC ->MODER |=(GPIO_MODER_MODE11_1);

GPIOC ->OTYPER &= ~(GPIO_OTYPER_OT_11); ///push pull output type for GPIOA12

GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR11_0); // high speed for GPPIOC12

GPIOC ->OSPEEDR |= (GPIO_OSPEEDER_OSPEEDR11_1);

GPIOC ->PUPDR &= ~(GPIO_PUPDR_PUPDR11); //NO PULL UP*/

GPIOC->AFR[1] |=(1<<28); //Alternate function 7 for PC10 USART TX

GPIOC->AFR[1] |=(1<<29);

GPIOC->AFR[1] |=(1<<30);

GPIOC->AFR[1] &=~(1<<31);

GPIOC->AFR[1] |=(1<<28); //Alternate function 7 for PC11 USART RX

GPIOC->AFR[1] |=(1<<29);

GPIOC->AFR[1] |=(1<<30);

GPIOC->AFR[1] &=~(1<<31);

Config_Lcd ();

Set_GPIOB_OutPut_No_Pu(9);

RCC->APB1ENR1 |= RCC_APB1ENR1_USART3EN; //enable USART3 clock

USART3->BRR =4000000/96; //baud rate = 9600

USART3->CR1&=~(1<<28); //1 Start bit, 8 data bits, n stop bits

USART3->CR1&=~(1<<12);

USART3->CR1 |= USART_CR1_UE; // USART3 enable.

USART3->CR1 |= (1<<3); // USART3 tx enable.

USART3->CR2 &= ~(1<<12); //1 stop bit

USART3->CR2 &= ~(1<<13); //1 stop bit

// USART3->CR1 = USART_CR1_RXNEIE | USART_CR1_RE | USART_CR1_UE;

char my_str[]='fooo';

__enable_irq(); //enable interrupt

NVIC_SetPriority(USART3_IRQn,4); //Set priority

NVIC_ClearPendingIRQ(USART3_IRQn); //clear pending

NVIC_EnableIRQ(USART3_IRQn);

while(1)

{

send_string(my_str); /* Will inititiate TC if TXE is set*/

USART3->RDR='a';

Delay_ms(1000);

Clear_Lcd();

Delay_ms(1000);

}

return 0;

}
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    March 28, 2018
    Posted on March 28, 2018 at 13:27

    Posted example code to other threads, might want to pay attention to error flags (framing, noise, parity) and clearing them.

    https://community.st.com/0D50X00009XkVxKSAV

     

    Sorry not digging into register level code

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..