Question
UART/USART Selection for a Serial Console on the STM32H533ZET6
We are designing a board based on the STM32H533ZET6 (LQFP144). We plan to implement a serial console in our application firmware to output debug logs (printf) and exchange commands and responses with a PC terminal.
Before finalizing the pin assignments, could you please confirm the following?
- Can we use any of the available serial peripherals—USART1, USART2, USART3, USART6, UART4, UART5, or LPUART1—for this console in asynchronous mode?
- If we select a valid TX/RX pin pair and configure the corresponding GPIO alternate functions, are there any additional restrictions or recommendations for this package? If so, please point us to the relevant documentation.
- Separately, if we want to use the built-in system memory (ROM) bootloader for firmware programming over UART, which USART instances and TX/RX pin pairs are supported on the STM32H533ZET6?