Skip to main content
phkloth
Associate II
August 22, 2022
Solved

UART Transmit Interrupt disable while keeping the Receive Interrupt alive

Hi all,

I have a question regarding the control of the UART interrupt on the STM32F4.

First let me describe the application:

int main(void)
{
 
SystemInit();
 
//Stream out Data via Uart via DMA
HAL_UART_Transmit_DMA(&huart2, (uint8_t *)UARTMessage_out, MSGLENGTH);	
//Enable UART Rx interrupt in order to receive messages over Terminal
HAL_UART_Receive_IT(&huart2, dataRx, 1);									
 
 /* Infinite loop */
 while (1)
 {
 
 ADCRead();
 Computations();
 DACWrite();
 
 //In this section the transmit Interrupt is allowed to fire
 HAL_NVIC_EnableIRQ(DMA1_Stream6_IRQn);
  if(DMAReady == 1)
 {
 GenerateUARTMsg();
 DMAReady=0;
 UART_DMA_Transmit()
 }
 //here the UART transmit interrupt again disabled
 HAL_NVIC_DisableIRQ(DMA1_Stream6_IRQn);
 
 }
 
}
 
//Callback when MCUout/PCin Message is done
//Here the time between two Messages is measured
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
 	timer = __HAL_TIM_GetCounter(&htim2);			
	__HAL_TIM_DISABLE(&htim2);
	__HAL_TIM_SetCounter(&htim2,0);					//reset counter back to zero
 	DMAReady = 0;								/
 	__HAL_TIM_ENABLE(&htim2);
 }
 
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
 ProcessInput();
HAL_UART_Receive_IT(&huart2, dataRx, 1);
 }

Somehow the disable of the DMA interrupt (HAL_NVIC_DisableIRQ(DMA1_Stream6_IRQn);) does not work.

When I disable the whole uart interrupt via HAL_NVIC_EnableIRQ(USART2_IRQn) it works. But then also the receive interrupt is disabled. But the receive interrupt is allowed to fire all the time.

Background:

Uart transmit interrupt is for monitoring the adc values. This process shall not interrupt the ADC->Compute->DAC routine.

UART receive changes compute parameters. For this, the Data cycle is allowed to be interrupted.

Thanks in advance for your help!

This topic has been closed for replies.
phkloth
phklothBest answer
Associate II
August 23, 2022

Ok I found the solution for this problem.

I use the macros:

 __HAL_UART_ENABLE_IT(&huart2,UART_IT_TC);

and the

 __HAL_UART_DISABLE_IT(&huart2,UART_IT_TC);

Here the arg UART_IT_TC:  Transmission complete interrupt.

It works in this context. I dont know however if this is the best solution.

2 replies

phkloth
phklothAuthor
Associate II
August 22, 2022

Ahh stupid.

Of course in the transmit callback the flag must be

DMAReady=1;

Somehow I cannot edit the first post?

phkloth
phklothAuthorBest answer
Associate II
August 23, 2022

Ok I found the solution for this problem.

I use the macros:

 __HAL_UART_ENABLE_IT(&huart2,UART_IT_TC);

and the

 __HAL_UART_DISABLE_IT(&huart2,UART_IT_TC);

Here the arg UART_IT_TC:  Transmission complete interrupt.

It works in this context. I dont know however if this is the best solution.