Skip to main content
moustaid jamal
Associate II
May 29, 2017
Question

UART PROBLEM

  • May 29, 2017
  • 1 reply
  • 609 views
Posted on May 29, 2017 at 15:26

Hi,

In my project i want to use two uart in the same card (stm32F4xx), the first UART (UART6) is connected with PC  and the seconde one (UART3) is connected with others cards.

It's possible to send via UART3 what i receive with UART6?? 

#uart #stm32
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
May 29, 2017
Posted on May 29, 2017 at 16:38

>>It's possible to send via UART3 what i receive with UART6?? 

Yes, you'd need to take the data received by one and send it out the other, if the baud rates are the same you might get away with just doing this in a loop, or via the IRQHandler. A more robust method would be to buffer the data to provide some elasticity.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..