Question
UART pins on STM32L4P5RE (LQFP64)
Hello,
I'm trying to understand the UART availability on the STM32L4P5RE in the LQFP64 package.
In the datasheet, Table 2 contains the note:
"For 48-pin and 64-pin packages only 1x UART is available."
I am not sure which UART this note refers to.
Looking at Table 15 (pin assignment), I can see:
- Pin 12: PA2 = USART2_TX
- Pin 13: PA3 = USART2_RX
and also:
- Pin 42: PA9 = USART1_TX
- Pin 43: PA10 = USART1_RX
This seems to indicate that both USART1 and USART2 pins are available on the package.
My questions are:
- Which UART is referred to by the "1x UART available" note in Table 2?
- Are both USART1 and USART2 functional on the STM32L4P5RE LQFP64 package?
- If only one UART is available, which instance is actually implemented?
- Is the note referring to a peripheral named UART4/UART5, while USART1 and USART2 remain available?
I would appreciate any clarification on how this note should be interpreted.
Thank you.