Skip to main content
fabricepeden
Associate III
February 22, 2013
Question

UART initialisation

  • February 22, 2013
  • 5 replies
  • 864 views
Posted on February 22, 2013 at 09:24

Hi everybody,

I'm using a STM32F205VE and something that I don't understand.

I do this :

  USART_InitStructure.USART_BaudRate = 9600;

  USART_InitStructure.USART_WordLength = USART_WordLength_8b;

  USART_InitStructure.USART_StopBits = USART_StopBits_1;

  USART_InitStructure.USART_Parity = USART_Parity_No;

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

  USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

  USART_Init(USART6,&USART_InitStructure);

and I can see the configuration into the USART6 register.

I do the same thing for USART3 and nothing happen, no registers are configurated.

Have you some ideas about this problem ? Must I do something special for this USART ?

Thank you in advance,

    This topic has been closed for replies.

    5 replies

    waclawek.jan
    Super User
    February 22, 2013
    Posted on February 22, 2013 at 09:33

     *          ===================================================================

      *                                 How to use this driver

      *          ===================================================================

      *          1. Enable peripheral clock using the follwoing functions

      *             RCC_APB2PeriphClockCmd(RCC_APB2Periph_USARTx, ENABLE) for USART1 and USART6

      *             RCC_APB1PeriphClockCmd(RCC_APB1Periph_USARTx, ENABLE) for USART2, USART3, UART4 or UART5.

    Tesla DeLorean
    Guru
    February 22, 2013
    Posted on February 22, 2013 at 09:43

    For synchronous designs, Rule#1 : Enable the clock.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    fabricepeden
    Associate III
    February 22, 2013
    Posted on February 22, 2013 at 09:50

    Sorry, I think I will post all my code, it would be easier for everybody.

     /* COM1 - NETWORK OUT */

      RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE);

      RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC,ENABLE);

      

      GPIO_PinAFConfig(EVAL_COM1_TX_GPIO_PORT,EVAL_COM1_TX_SOURCE,EVAL_COM1_TX_AF);

      GPIO_PinAFConfig(EVAL_COM1_RX_GPIO_PORT,EVAL_COM1_RX_SOURCE,EVAL_COM1_RX_AF);

      

      /* Configure USART Tx and Rx as alternate function push-pull */

      GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

      GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

      GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

      GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

      GPIO_InitStructure.GPIO_Pin = EVAL_COM1_TX_PIN;

      GPIO_Init(EVAL_COM1_TX_GPIO_PORT, &GPIO_InitStructure);

      

      GPIO_InitStructure.GPIO_Pin = EVAL_COM1_RX_PIN;

      GPIO_Init(EVAL_COM1_RX_GPIO_PORT, &GPIO_InitStructure);

      

      /* Configuration : 115200 bauds, 8 N 1 */

      USART_InitStructure.USART_BaudRate = 115200;

      USART_InitStructure.USART_WordLength = USART_WordLength_8b;

      USART_InitStructure.USART_StopBits = USART_StopBits_1;

      USART_InitStructure.USART_Parity = USART_Parity_No;

      USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

      USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

      

      /*USART_OverSampling8Cmd(EVAL_COM1,ENABLE);*/

      

      USART_Init(EVAL_COM1,&USART_InitStructure);

     

      /* Enable the USARTx Interrupt */

      NVIC_InitStructure.NVIC_IRQChannel = EVAL_COM1_IRQn;

      NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

      NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

      NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

      NVIC_Init(&NVIC_InitStructure);

      

      USART_ITConfig(EVAL_COM1, USART_IT_TXE, DISABLE);

      USART_ITConfig(EVAL_COM1, USART_IT_RXNE, ENABLE);

      

      /* Enable USART */

      USART_Cmd(EVAL_COM1, ENABLE);

      

      /* Configuration de la PIN REDE */

      COMRDInit(COM1);

      

      /* COM2 - NETWORK IN */

      /* COM1 - NETWORK OUT */

      RCC_APB2PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);

      RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD,ENABLE);

      

      GPIO_PinAFConfig(EVAL_COM2_TX_GPIO_PORT,EVAL_COM2_TX_SOURCE,EVAL_COM2_TX_AF);

      GPIO_PinAFConfig(EVAL_COM2_RX_GPIO_PORT,EVAL_COM2_RX_SOURCE,EVAL_COM2_RX_AF);

      

      /* Configure USART Tx and Rx as alternate function push-pull */

      GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

      GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

      GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

      GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

      GPIO_InitStructure.GPIO_Pin = EVAL_COM2_TX_PIN;

      GPIO_Init(EVAL_COM2_TX_GPIO_PORT, &GPIO_InitStructure);

      

      GPIO_InitStructure.GPIO_Pin = EVAL_COM2_RX_PIN;

      GPIO_Init(EVAL_COM2_RX_GPIO_PORT, &GPIO_InitStructure);

      

      /* Configuration : 115200 bauds, 8 N 1 */

      USART_InitStructure.USART_BaudRate = 9600;

      USART_InitStructure.USART_WordLength = USART_WordLength_8b;

      USART_InitStructure.USART_StopBits = USART_StopBits_1;

      USART_InitStructure.USART_Parity = USART_Parity_No;

      USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

      USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

      USART_Init(EVAL_COM2,&USART_InitStructure);

     

      /* Enable the USARTx Interrupt */

      NVIC_InitStructure.NVIC_IRQChannel = EVAL_COM2_IRQn;

      NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F;

      NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F;

      NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

      NVIC_Init(&NVIC_InitStructure);

      

      USART_ITConfig(EVAL_COM2, USART_IT_TC, ENABLE);

      USART_ITConfig(EVAL_COM2, USART_IT_RXNE, ENABLE); 

      

      /* Enable USART */

      USART_Cmd(EVAL_COM2, ENABLE);

      

      /* Configuration de la PIN REDE */

      COMRDInit(COM2);
    waclawek.jan
    Super User
    February 22, 2013
    Posted on February 22, 2013 at 11:04

    >   RCC_APB2PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);

     *          ===================================================================

      *                                 How to use this driver

      *          ===================================================================

      *          1. Enable peripheral clock using the follwoing functions

      *             RCC_APB2PeriphClockCmd(RCC_APB2Periph_USARTx, ENABLE) for USART1 and USART6

      *             RCC_APB1PeriphClockCmd(RCC_APB1Periph_USARTx, ENABLE) for USART2, USART3, UART4 or UART5.

    JW

    fabricepeden
    Associate III
    February 22, 2013
    Posted on February 22, 2013 at 15:24

    Thank you for your answer.

    Now my registers are well configured.

    I'll see if my UART is working !