Uart DMA RX problem
Hi there !
I use uart with DMA for receive data from (right now) pc and STM32F051 discovery board, everythingh work bettere if i send all data, but if i send less data stop the work . Let me explain i need the send 180 bytes from pc to discovery board , i know i can have two interrupt one for HC (half comunication)e the other for TC(total comunications) but if i send 4 byte i diden't receive any interrupt, but the problem is the pointer of the counter don't start from 0 to put the data inside the buffer (configurarte in circular mode) but start from the 5 position. Some one have any idea how i can fix this problem ?
Thank you soo much
Sergio