Skip to main content
Senior
March 14, 2024
Solved

UART data receive acknowledgement

Two devices A & B are communicating on UART. A sends data stream to B. B sends one byte data back to A to acknowldge that data has been received. 

I want to implement if A doesn't receive acknowledgement from B then it display Error message on LCD.

Please suggest best logic in A to implement this.

As far I think I should start the UART_Receive_IT API for one byte . and complete callback sets the flag for acknowlegement. Incase flag is not set within one second or so after sending data then A display Error message on LCD. Should I start HAL_Delay(1000) after sending data and then check for flag set or not?

If anyother best way, kindly suggest. 

I am still relatively new to coding word..so trying to find best ways.. ;)

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
March 14, 2024

The blocking HAL_UART_Receive() API takes a timeout:

AndrewNeil_0-1710437312958.png

the non-blocking HAL_UART_Receive_IT() doesn't:

AndrewNeil_1-1710437344915.png

 

Using HAL_Delay() effectively makes your code blocking - so there seems no point in using the non-blocking API?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

4 replies

Tesla DeLorean
Guru
March 14, 2024

>>Should I start HAL_Delay(1000) after sending data and then check for flag set or not?

No, you'd do better taking a TickCount, say HAL_GetTick(), and use that to determine if enough time has expired without getting a callback with the acknowledgment byte 

If it responds more quickly you can proceed to do other things.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Andrew NeilBest answer
Super User
March 14, 2024

The blocking HAL_UART_Receive() API takes a timeout:

AndrewNeil_0-1710437312958.png

the non-blocking HAL_UART_Receive_IT() doesn't:

AndrewNeil_1-1710437344915.png

 

Using HAL_Delay() effectively makes your code blocking - so there seems no point in using the non-blocking API?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Nico3Author
Senior
March 14, 2024

Cool,

So after sending data , i run the blocking HAL_UART_Receive()with timeout of say 1 second and then check the HAL_StatusTypeDef return. 

 

Andrew Neil
Super User
March 14, 2024

Yes.

And, of course, check the received character (if any) - to make sure it's the correct acknowledgement.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.