Skip to main content
explorinova
Associate
March 7, 2012
Question

UART connection

  • March 7, 2012
  • 5 replies
  • 1020 views
Posted on March 07, 2012 at 10:13

I wanted to

use the

UART port

but can not find

any information

to use this port

,

the port

only appears to

USART

, does anyone

can give me

some tips

how you can

connect the

stm32f4discovery

to establish

contact with

this type of

port (

UART

)

#espn
    This topic has been closed for replies.

    5 replies

    ronandouguet
    Associate III
    March 7, 2012
    Posted on March 07, 2012 at 11:24

    Hi,

    Here an example to configure and use UART 3 :

    /**************************************************************************
    * @descr Initialise UART3 - RX:PD9 et TX:PD8
    * @param None
    * @retval None
    *************************************************************************/
    void
    UART3Init(
    void
    )
    {
    USART_InitTypeDef UART3_InitStructure;
    GPIO_InitTypeDef GPIO_InitStructure;
    /* Enable USART3 clock */
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
    /* Connect PD8 and PD9 pins to AF */
    GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_USART3);
    GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_USART3);
    /* Configure USART3 Tx (PD8) as input floating */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_Init( GPIOD, &GPIO_InitStructure );
    /* Configure USART3 Rx (PD9) as input floating */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_Init( GPIOD, &GPIO_InitStructure );
    /* Initialise Structure UART3 */
    UART3_InitStructure.USART_BaudRate = 9600;
    UART3_InitStructure.USART_WordLength = USART_WordLength_8b;
    UART3_InitStructure.USART_StopBits = USART_StopBits_1;
    UART3_InitStructure.USART_Parity = USART_Parity_No;
    UART3_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
    UART3_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
    /* Initialise UART3 */
    USART_Init(USART3,&UART3_InitStructure);
    /* Enable the interrupt Rx UART3 */
    USART_ITConfig(USART3, USART_IT_RXNE, ENABLE);
    /* Enable the UART3 */
    USART_Cmd( USART3, ENABLE );
    }
    /**************************************************************************
    * @descr Envoie d'un caractere via l'UARTx
    * @param USARTx definie l'uart à utiliser (1,2,3,4,5,6)
    * @param Data caractere à transferer
    * @retval None
    *************************************************************************/
    void
    USART_SendChar(USART_TypeDef* USARTx, unsigned 
    char
    Data)
    {
    /* Check the parameters */
    assert_param(IS_USART_ALL_PERIPH(USARTx));
    /* Transmit Data */
    USARTx->DR = (Data & (uint16_t)0x01FF);
    }
    /**************************************************************************
    * @descr Envoie d'une chaine de caracteres via l'UARTx
    * @param USARTx definie l'uart à utiliser (1,2,3,4,5,6)
    * @param s chaine de caracteres à transferer
    * @retval None
    *************************************************************************/
    void
    USART_SendString(USART_TypeDef* USARTx, 
    char
    *s)
    {
    /* Check the parameters */
    assert_param(IS_USART_ALL_PERIPH(USARTx));
    while
    (*s)
    {
    while
    (USART_GetFlagStatus(USARTx, USART_FLAG_TXE) == RESET);
    USART_SendData(USARTx, *s++);
    }
    }

    Tesla DeLorean
    Guru
    March 7, 2012
    Posted on March 07, 2012 at 18:57

    I wanted to

     

    use the

     

    UART port

     

    but can not find

     

    any information

     

    to use this port

    ,

     

    the port

    only appears to

     

    USART

    , does anyone

     

    can give me

     

    some tips

     

    how you can

     

    connect the

    stm32f4discovery

     

    to establish

     

    contact with

     

    this type of

     

    port (

    UART

    )

    The easiest way to get serial to a PC is via a USB-to-CMOS Serial chip/cable from the likes of FTDI, Silicon Labs or Prolific. Basically hook up TX, RX and GND, to a USART of your choice. USART3 would be recommended, use the pins supported by the boot loader.

    To connect to RS232 level serial, you'll need a MAX232 type device to buffer the voltages.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    explorinova
    Associate
    March 12, 2012
    Posted on March 12, 2012 at 12:30

    but I

    'm

    trying to communicate with

    one

    Wifi

    module

    that has only

    one

    UART port

    for communication

    and I am not

    able to transmit.

     

    zaurozavr
    Visitor II
    March 12, 2012
    Posted on March 12, 2012 at 14:30

    Any USART port can work as UART if you add

    USARTX_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
     in port initialization.
     BTW some WIFI modules require USARTfor the high speed only (> 115200).
     

    Tesla DeLorean
    Guru
    March 12, 2012
    Posted on March 12, 2012 at 14:54

    but I

    'm

    trying to communicate with

    one

    Wifi

    module

    that has only

    one

    UART port

    for communication

    and I am not

    able to transmit.

    Unfortunately your posts don't contain enough specific detail, and I don't have time to guess what might be wrong. None of us know what you are doing, you have to explain in more detail.

    What module?

    How's it connected?

    What pins?

    What USART?

    How's the software configured?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..