Skip to main content
Associate II
Nov 17, 2025 1:25 PM UTC
Question

UART bootloader mode does not work after the board has been programmed

Dear Sir,

My board is equipped with STM32G431 MCU. 

I found that the UART DFU mode of my board does not work after the flash of the MCU has been programmed. The UART DFU mode can only work with a blank MCU that have not been programmed before. I have only used the default setting in the CubeProgrammer.

I appreciate if you can give me any suggestion.

12 replies

mƎALLEm
ST Technical Moderator
Nov 17, 2025 1:35 PM UTC

Hello @teddyw and welcome to the ST community,

There is no UART DFU mode. They are separated things: DFU: bootloader over USB and bootloader over UART.

So you mean the bootloader over UART?

You need to provide the exact steps you followed to program the MCU with the ST bootloader.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
teddywAuthor
Associate II
Nov 17, 2025 1:51 PM UTC

I have no idea it is DFU or Bootloader UART. I am just using CubeProgrammer UART to communicate with the board. ST has doc mentioning about DFU and bootstrap. Please clarify.  

teddywAuthor
Associate II
Nov 17, 2025 1:56 PM UTC

Hi,

I have set the BOOT0 pin to high during power up then what mode should the MCU go into ?

Is it bootstrap or DFU ?

ST Technical Moderator
Nov 17, 2025 1:36 PM UTC

Hi @teddyw 

Do you have the same issue with reference board?

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate
Nov 17, 2025 3:22 PM UTC

It sounds like your application code may be changing the boot configuration or blocking the bootloader from starting. Check your option bytes, especially BOOT0 and nBOOT_SEL, and make sure the user code isn’t disabling the system bootloader. Also confirm the UART pins are free at reset. If DFU only works when the MCU is blank, it usually means the boot mode settings are being overwritten once the firmware is flashed.

teddywAuthor
Associate II
Nov 24, 2025 10:05 AM UTC

I have already check the OB. It is the same as the virgin new board.

teddyw_0-1763978543927.pngteddyw_1-1763978581390.png

It looks like there is something else causing the programmed board having difficulty to start communication with the UART bootloader.